Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
ADC-Architecture-Slide8

Early SAR ADCs used thin film laser wafer trimmed internal DACs. Today, this approach has been replaced by switched capacitor (charge redistribution) CMOS DACs shown here. The capacitor matching is controlled by the precise lithography, and extra capacitors and switches can be added for trimming either at the factory or as part of autocalibration routines run at the system level after installation. Note that switch SIN performs the sample-and-hold (SHA or SAH) function so no additional SHA is needed. Drawbacks to this architecture include the switching transient currents injected on the analog input which requires the drive circuitry to tolerate these transient currents without loss of accuracy.

PTM Published on: 2007-10-05