The Role of Power Relays in Reliable HVAC System Design

Af Nick Grillone, Applications Engineer, Same Sky

Power relays form the electrical boundary between low-voltage control electronics and the high-power loads that perform real work in HVAC systems. When a thermostat signals a compressor start, an indoor blower ramps up, or auxiliary heat engages, a relay must translate that control command into a safe, repeatable power transition. These switching events occur under demanding electrical and environmental conditions, making relay selection a key design decision.

HVAC equipment routinely encounters high motor inrush currents, wide temperature swings, elevated humidity, and frequent switching cycles. As adoption of air conditioning and heat pump systems continues to rise—driven by electrification initiatives, climate trends, and energy-efficiency mandates—expectations for reliability and service life are increasing in parallel. Standards such as SEER, HSPF, and regional energy codes further pressure designers to reduce parasitic losses, control thermal rise on PCBs, and maintain consistent electrical performance over years of operation.

How relays function within HVAC architectures

At a system level, relays act as controlled isolation devices that allow low-power logic circuits to manage high-voltage or high-current loads. Large loads such as compressors are often switched using panel-mounted contactors, while PCB-mounted relays handle functions including indoor fans, heaters, pumps, and valves.

Control voltage conventions vary widely. In many North American systems, 24 VAC control loops remain common, while newer inverter-driven platforms increasingly rely on low-voltage DC control (typically 5 V or 12 V). These differences influence coil selection, pickup and dropout margins, and overall control-board efficiency. In multi-region designs, validating relay operation across voltage tolerances and brownout conditions is critical to prevent failures or incomplete switching events.

Although factors like coil type or contact material may appear secondary during early design stages, they directly affect energy consumption, electrical noise, and long-term reliability once systems are deployed in the field.

Electrical stress and the impact of inrush current

One of the most significant stressors for HVAC relays is motor inrush current. Compressors and fan motors can draw several times their rated steady-state current during startup. When relay contacts close under these conditions, electrical arcing occurs as contacts transition from open to closed. Over time, this arcing degrades contact surfaces, increases contact resistance, and raises localized temperatures.

Contact bounce during closure further intensifies arcing, accelerating wear and shortening operational life. For this reason, HVAC relays frequently employ contact materials such as silver tin oxide, which provide improved resistance to welding and erosion when switching inductive loads.

Diagram of electrical arcing caused by inductive switchingFigure 1: Electrical arcing caused by inductive switching accelerates contact wear and reduces relay service life. (Image source: Same Sky)

While inverter-driven compressors reduce startup stress by gradually ramping motor speed, relays are still heavily utilized elsewhere in the system. Reversing valves, auxiliary heaters, pumps, and defrost circuitry may switch frequently, and even moderate inductive loads can generate damaging voltage transients if not properly managed with suppression components such as RC snubbers or varistors.

Common HVAC applications for power relays

Relays are distributed throughout HVAC systems, supporting both primary and secondary functions. Condenser fans and indoor blowers are typical relay-driven loads, requiring components that tolerate repetitive cycling and inductive stress. Although these motors consume less power than compressors, their frequent operation makes mechanical endurance and contact stability essential.

In heat pump systems, relays often control reversing-valve solenoids, which determine refrigerant flow direction between heating and cooling modes. Precise switching is required to avoid pressure imbalances that could compromise system efficiency or reliability.

Relays also manage resistive loads such as crankcase heaters and electric heat strips. These components may operate continuously or in staged configurations, demanding relays capable of carrying high steady-state currents without excessive temperature rise. Additional functions, such as condensate pumps, humidifiers, and auxiliary accessories, further illustrate how relays serve as critical enablers across the HVAC platform.

Key design considerations for HVAC relay selection

Electrical ratings must be evaluated beyond nominal load current. Designers must account for startup surges, locked-rotor conditions, and worst-case fault scenarios. In many cases, the most severe electrical stress occurs during contact opening, when inductive energy generates sustained arcing that challenges contact integrity.

Environmental exposure is equally important. HVAC equipment may operate in rooftop enclosures, basements, or outdoor units where temperatures range from sub-zero winter conditions to elevated summer heat. Moisture, condensation, and airborne contaminants can further degrade performance if housings and insulation systems are not adequately designed.

Control strategy also influences relay choice. AC-driven coils, DC coils, and mains-referenced logic each introduce tradeoffs related to efficiency, EMI, and thermal management. Early alignment with regulatory requirements, such as UL and IEC standards governing creepage, clearance, and material flammability, helps avoid late-stage redesigns and certification delays.

Relay challenges unique to air-source heat pumps

Air-source heat pumps place additional demands on relay performance due to their operating complexity. Reversing valves must be actuated in coordination with compressors and fans, requiring consistent timing and reliable switching under varying load conditions.

Electric auxiliary heaters introduce high-current switching events, often in multi-stage configurations. Relays controlling these elements must handle sustained current without excessive contact heating or mechanical degradation.

Defrost cycles further increase relay activity. During cold-weather operation, systems periodically reverse operation to clear frost from outdoor coils, requiring multiple coordinated switching events. Fixed-speed compressors experience higher inrush currents at low temperatures, compounding electrical stress during these cycles.

To reduce standby power consumption, many modern designs incorporate low-power or latching relays at the control-board level. While these approaches improve system efficiency, designers must still account for downstream loads, such as reversing-valve solenoids, that require continuous power once energized.

A practical relay selection framework

A structured evaluation approach simplifies relay selection for HVAC applications. Key criteria include electrical ratings under surge conditions, environmental robustness, coil efficiency, regulatory compliance, and mechanical endurance. Reviewing these factors early in the design process helps ensure reliable performance across the system’s full operating life. Table 1 below outlines these in greater detail.

Consideration Details
Load review Account for motor power, resistive heater loads, separate make/break ratings, and inrush or locked rotor amperage (LRA).
Voltage and frequency Confirm compatibility with supply conditions (e.g., 120 VAC, 240 VAC, 24 VAC, DC, single-phase, or three-phase). Match relay ratings to the most common standards in the target market.
Environmental conditions Assess expected ambient temperatures and enclosure exposure. Choose insulation, sealing, and materials suitable for humidity, condensation, and contaminants.
Regulatory compliance Verify adherence to UL, IEC, and other applicable standards covering safety, creepage/clearance, and flammability.
Serviceability Consider whether relays are field-replaceable and how easily technicians can access and interact with them during maintenance.
Coil design Ensure the coil type aligns with the intended mode of operation and that coil power requirements are compatible with the control system.

Table 1: Relay selection checklist for HVAC. (Image source: Same Sky)

Closing thoughts

Power relays may appear to be small components within an HVAC system, but their influence on reliability, efficiency, and service life is substantial. As HVAC designs evolve toward higher efficiency and increased electrification, relay performance becomes even more critical. Treating relays as core design elements rather than interchangeable commodities results in systems that switch cleanly, operate efficiently, and withstand years of demanding service. Same Sky’s broad portfolio of power relays supports these requirements across a wide range of HVAC applications.

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.

Om denne forfatter

Image of Nick Grillone

Nick Grillone, Applications Engineer, Same Sky

Nick Grillone brings over 10 years of customer support experience to the Same Sky's Applications Engineering team. His technical and application expertise is particularly focused on our diverse range of audio components, such as microphones and speakers, as well as our sensor technology offering. In his spare time, Nick enjoys all things outdoors with his partner and his dog, including backpacking, camping, cycling, and paddleboarding.