Ordrerne leveres typisk til Danmark inden for 48 timer , afhængig af lokation.
Gratis levering til Danmark på ordrer med mindst kr. 340 Et leveringsgebyr på kr. 135 faktureres for alle ordrer mindre end kr. 340.
UPS eller FedEx fragt forudbetalt: DDP (Told og afgifter betales af DigiKey)
DHL fragt forudbetalt: CPT (told, afgifter og moms betales ved levering)
Kreditkonto for kvalificerede institutioner og virksomheder
Forudbetaling via bankoverførsel
![]()
![]()
![]()
![]()


Flere produkter fra fuldt autoriserede partnere
Gennemsnitlig forsendelsestid på 1-3 dage. Der kan være pålagt ekstra gebyrer på forsendelsen. Se produktsiden, indkøbskurven og kassen for at se den faktiske forsendelsestid.
Incoterms: CPT (told og moms forfalder på leveringstidspunktet)
For mere information, besøg Hjælp og support
It's blue! It's thin! It's the Arduino Pro Mini! SparkFun's minimal design approach to Arduino. This is a 3.3V Arduino running the 8MHz bootloader. Arduino Pro Mini does not come with connectors populated so that you can solder in any connector or wire with any orientation you need.
The TM4C123G LaunchPad Evaluation Kit is a low-cost evaluation platform for ARM Cortex-M4F based microcontrollers from Texas Instruments. The design of the TM4C123G LaunchPad highlights the TM4C123GH6PM microcontroller with a USB 2.0 device interface and hibernation module.
In 2015 we developed the BadgerStick as a fun and interactive way for people to learn about soldering and engage with SparkFun products at the multiple trade shows we appeared at. In 2016 we have refined the BadgerStick into what you see here, the SparkFun RedStick! The RedStick combines some of our favorite features like the Uno's Optiboot bootloader, the FTDI, small size, and the ability to plug directly into a computer's USB port (no FTDI board or USB cable required).
The SparkFun ESP32 Thing is a comprehensive development platform for Espressif’s ESP32, their super-charged version of the popular ESP8266. Like the 8266, the ESP32 is a WiFi-compatible microcontroller, but to that it adds support for Bluetooth low-energy (i.e BLE, BT4.0, Bluetooth Smart), and nearly 30 I/O pins. The ESP32’s power and versatility will make it the foundation of IoT and connected projects for many years to come.
Measuring approx 1" x 6" standard-thickness FR4, this gold plated ruler has the most common component packages you'll encounter. It also has font size guide, trace-width diagram, and a set of schematic symbol guides so you can keep track of your transistor pinouts. Embedded in the end is a Trinket M0, our little Cortex M0+ development board, and in addition, there are 4 capacitive touch pads with matching LEDs that our code will turn into a specialized engineer keyboard.
The Arduino Nano is a compact board similar to the UNO., but in a much smaller form factor making it perfect for breadboarding or projects where size is important.
The HUZZAH32 is our ESP32-based Feather, made with the official WROOM32 module. We packed everything you love about Feathers: built in USB-to-Serial converter, automatic bootloader reset, Lithium Ion/Polymer charger, and just about all of the GPIOs brought out so you can use it with any of our Feather Wings.
ESP32-PICO-KIT is an ESP32-based mini development board produced by Espressif. The core of this board is ESP32-PICO-D4 - a System-in-Package (SiP) module with complete Wi-Fi and Bluetooth functionalities. Compared to other ESP32 modules, ESP32-PICO-D4 integrates peripheral components in one single package, which otherwise would need to be installed separately.
This is the Adafruit Feather M0 Adalogger - our take on an 'all-in-one' Cortex M0 datalogger (or data-reader) with built in USB and battery charging. It's an Adafruit Feather M0 with a microSD holder ready to rock!
It's blue! It's thin! It's the Arduino Pro Mini! SparkFun's minimal design approach to Arduino. This is a 5V Arduino running the 16MHz bootloader. Arduino Pro Mini does not come with connectors populated so that you can solder in any connector or wire with any orientation you need.
Tak!
Hold øje med din indbakke for nyheder og opdateringer fra DigiKey!
Indtast en e-mailadresse
Accepter venligst afkrydsningsfeltet