Maker.io main logo

Add Time of Flight Sensor to Arduino Due

294

2020-12-02 | By Digilent Inc

License: None Arduino

The Pmod ToF is an optical distance measuring device, which contains the ISL29501 on-chip digital signal processor. After calibration, measurements can be taken by sending a low pulse on the Sample Start (SS) line. If the proper jumper is set, the device pulls the Interrupt (IRQ) line to low, when the data is ready. The measured distance in meters data are transmitted through the I2C interface in two bytes. The range of the sensor is 5m. It has low power consumption and is operated by 3.3V power source. So, you can source the power from the Arduino Due.

Specifications

Pmod ToF also has an EEPROM which the user- and factory calibration values are stored. When calibrating, the values can be retrieved from this memory, or after a calibration, the newly acquired values can be saved here. The memory is structured in four parts: 

EEPROM structure

The address of the Pmod ToF I2C interface is 0x57 and the address of the EEPROM is 0x50. The maximum supported serial clock frequency is 400KHz.The Pmod has jumpers for enabling pull-up resistors on the Serial Clock (SCL) and Serial Data (SDA) lines, as well as two pin headers (male and female), which allow daisy-chaining.  Here is the pinout:

Pinout

Calibrate Pmod ToF

In this example, the Pmod will be used in single shot mode which it measures once after every request. Before taking the measurement, The SS line must be set as output and the IRQ line as the input. Control registers 0x10, 0x11, 0x13, 0x18, 0x19, 0x60, 0x90, 0x91 must be loaded with the values (see below table). You can also refer to the on-chip signal processor's datasheet.

Control register values

Now, you can calibrate the Pmod ToF by loading the correct values into registers 0x24 to 0x30. If you use the factory calibration values, you can load these values from the EEPROM. Otherwise, three phases of calibration have to be performed:

  • Magnitude calibration: It compensates the emitter currents. No action have to be taken while calibrating. Results are saved in registers 0x2C-0x2E.
  • Crosstalk calibration: Compensates for electrical crosstalk observed by the photodiode. At close range a large return signal values for crosstalk has a minor impact on distance measurements. At the far end of the distance range, the crosstalk might exceed the signal, adding significant error to measurements. In order to perform this calibration, the receiver or both optics need to be covered with the foam included in the package to make sure there is no return path for the IR signal emitted by the LED. If the optics are not correctly covered, it will result in large errors when measurements are taken. During this process, registers 0x24 to 0x2B are changed.
  • Distance calibration: Compensates for variation in delay of the emitter, photodiode, and the ISL29501 that will change the signal path delay. It will create a coefficient that will be subtracted in each measurement. For this calibration the user must set a predefined distance for which the calibration is performed. A good calibration at 1.5m can result in the ability of the Pmod ToF to measure up to 5 meters with an error of only a few centimeters. The calibrations should be performed at smaller distances (below 1.5m) to avoid distortion and noise that can affect the calibration. In order to perform the distance calibration, a white target (a target with high IR reflective capacity) should be placed at the desired distance from the Pmod ToF. The Pmod should be also placed at least 40cm above the ground or table and no objects should be within the +/-3° area of the optics. The farther the measurement is taken from the ToF, the bigger the area should be. During distance calibration registers 0x2F and 0x30 are changed.

Take the Measurement

To start a measurement, registers 0x13 and 0x60 must be set (single shot mode and interrupt on data ready) and register 0x69 should be addressed (clear interrupt when reading). The SS line should be held low for 5.6ms and then pulled-up. The IRQ line is pulled down when the measurement is complete. Results are stored in registers 0xD1 (MSB) and 0xD2 (LSB). The resulting number gives the distance in meters.

Connect the Arduino Due board to the Pmod ToF as follows:

  • 3V3 on Arduino to VCC on Pmod Tof
  • GND on Arduino to GND on Pmod ToF
  • SDA (20) on Arduino to SDA on Pmod ToF
  • SCL (21) on Arduino to SCL on Pmod ToF
  • 3, or any other digital pin on Arduino to SS on Pmod ToF
  • 2, or any other digital pin on Arduino to IRQ on Pmod ToF
  • Note: put all four jumpers on place on Pmod ToF

Wiring diagram

 

Results after running user calibration:

Results

The code:

https://create.arduino.cc/editor/almos_vv/c63a352a-d071-4e38-a4a1-9499890f39c2/preview

Copy Code
/************************************************************************

Distance measurement using Pmod ToF and Arduino Due

*************************************************************************

Description: Pmod_ToF, Arduino_Due
The Pmod can be user calibrated, or the default calibration values can be used.
After calibration, distance measurements are performed

Material
1. Arduino Due
2. Pmod ToF

Wiring
Pmod <----------> Arduino
VCC to 3V3
GND to GND
SDA to 20(SDA)
SCL to 21(SCL)
SS to 3
IRQ to 2(INT4)

Connect all 4 jumpers on the Pmod, to activate the SS and IRQ signals and the pull-ups on the I2C lines.

************************************************************************/

//define connections
#define IRQ 2 //interrupt at data ready
#define SS 3 //sample start

//define measurement unit (uncomment the chosen unit - default: CM)
#define CM //output in cm
//#define MM //output in mm
//#define INCH //output in inch

//is calibration required?
#define USER_CALIBRATION true //the user wants to recalibrate the sensor
#define FACTORY_CALIBRATION false //default calibration data restoring
//note: if both calibration types are set to false, the user calibration data will be loaded
#define CALIBRATION_DISTANCE 0.15 //actual distance on which the sensor is calibrated (in meters)

/*------------------------------------------------------------------------*/

//include headers
#include <Wire.h> //library for I2C communication
#include <math.h> //library for mathematical functions

/*------------------------------------------------------------------------*/

//define I2C parameters
#define i2c_address 0x57 //i2c address of the pmod
#define i2c_EEPROM 0x50 //i2cc address of the EEPROM
#define i2c_frequency 100 //communication frequency in KHz

//define EEPROM addresses
#define EEPROM_factory 0x20 //factory calibration data starting address
#define EEPROM_user 0x10 //user calibration data starting address

/*------------------------------------------------------------------------*/

//factory calibration values
unsigned char ctrl_registers[] = {0x10, 0x11, 0x13, 0x60, 0x18, 0x19, 0x90, 0x91}; //used control register addresses
unsigned char cali_registers[] = {0x24, 0x25, 0x26, 0x27, 0x28, 0x29, 0x2A, 0x2B, 0x2C, 0x2D, 0x2E, 0x2F, 0x30}; //used calibrationregister addresses
unsigned char ctrl_values[] = {0x04, 0x6E, 0x71, 0x01, 0x22, 0x22, 0x0F, 0xFF}; //default control register values

/*------------------------------------------------------------------------*/

//function prototypes
void ToF_begin(void); //initializes the sensor
void ToF_start(void); //starts a measurement
float ToF_getMeasurement(void); //displays the measured distance on the serial monitor
void display_unit(void); //display the measurement unit on the serial monitor
void ToF_calibrate(void); //calibrate the sensor
void ToF_calibrate_magnitude(void); //perfomr magnitude calibration
void ToF_calibrate_crosstalk(unsigned int avg_nr = 100); //performe crosstalk calibration
void ToF_calibrate_distance(unsigned int reference_distance, unsigned int avg_nr = 100); //perform distance calibration
unsigned char read_reg(unsigned char reg); //read a register
void write_reg(unsigned char reg, unsigned char val); //write a register
void double2bytes(double nr, unsigned char *exp, unsigned char *msb, unsigned char *lsb); //convert a double to bytes
double bytes2double(unsigned char exp, unsigned char msb, unsigned char lsb); //convert 3 bytes to double
void debug(void); //display all registers
void EEPROM_read(unsigned char address); //read values from EEPROM
void EEPROM_write(unsigned char address); //write data to EEPROM

/*------------------------------------------------------------------------*/

void setup()
{
Serial.begin(9600); //initialize serial communication
Serial.println("Starting..."); //display a message

pinMode(SS, OUTPUT); //set pin as output
digitalWrite(SS, HIGH); //don't start a measurement yet
pinMode(IRQ, INPUT_PULLUP); //set pin as input
delay(1000); //allow power up

ToF_begin(); //initialize the pmod
//debug(); //display all registers
delay(1000); //wait one second (make the message readable)
}

/*------------------------------------------------------------------------*/

void loop()
{
Serial.println(); //leave a line out
Serial.println("Measurement started"); //display a message
float distance = ToF_getMeasurement(); //get distance
Serial.print("distance: "); //output a message
Serial.print(distance); //output the result
display_unit(); //display measurement unit
delay(3000); //wait 3s until the next measurement
}

/*------------------------------------------------------------------------*/

/*
initializes the sensor in default mode
arguments: nothing
returns: nothing
*/
void ToF_begin(void)
{
Wire.begin(); // initialization of I2C bus
Wire.setClock(i2c_frequency * 1000); // set communication frequency

write_reg(0x01, 0x00); //enable the chip
write_reg(0xB0, 0xD1); //soft clear - reset all registers, stop conversions

for (int i = 0; i < 8; i++) //load the first 8 register from the list to initialize the sensor
{
write_reg(ctrl_registers[i], ctrl_values[i]); //load the register
}
Serial.println("Initialization finished"); //display a message

if (USER_CALIBRATION) //calibrate the sensor
{
ToF_calibrate(); //calibrate the sensor
Serial.println("The sensor is calibrated"); //display a message
}
else if (FACTORY_CALIBRATION) //resotre default calibration settings
{
EEPROM_read(EEPROM_factory); //read factory calibration data
Serial.println("Factory calibration settings restored"); //display a message
}
else //load user calibration data
{
EEPROM_read(EEPROM_user); //read user calibration data
Serial.println("User calibration settings restored"); //display a message
}
return;
}

/*------------------------------------------------------------------------*/

/*
starts a measurement
arguments: nothing
returns: nothing
*/
void ToF_start(void)
{
//setup single shot mode
write_reg(0x13, 0x7D); //load the register

//enable interrupt
write_reg(0x60, 0x01); //load the register

//read clears interrupt
read_reg(0x69); //address the register

digitalWrite(SS, LOW); //initiate a measurement
delayMicroseconds(5600); //wait 5.6 ms
digitalWrite(SS, HIGH); //reset pin state
delayMicroseconds(14400); //wait 14.4 ms
return;
}

/*------------------------------------------------------------------------*/

/*
displays the measured distance on the serial monitor
arguments: nothing
returns: the distance
*/
float ToF_getMeasurement(void)
{
ToF_start(); //initialize measurement
while (digitalRead(IRQ) != 0)
; //wait for data

unsigned char MSB = read_reg(0xD1);
unsigned char LSB = read_reg(0xD2);

float distance = (((double)MSB * 256 + (double)LSB) / 65536) * 3331; //convert measured data

//convert the result if required
#if defined(INCH)
distance /= 2.54; //convert to inch
#elif defined(MM)
distance *= 10; //convert to mm
#endif

return distance;
}

/*------------------------------------------------------------------------*/

/*
displays the measurement unit on the serial monitor
arguments: none
returns: none
*/
void display_unit(void)
{
//inch
#ifdef INCH
Serial.println(" inch"); //dispay message
return;
#endif

//cm
#ifdef CM
Serial.println(" cm"); //dispay message
return;
#endif

//mm
#ifdef MM
Serial.println(" mm"); //dispay message
return;
#endif
}

/*------------------------------------------------------------------------*/

/*
calibrates the Pmod ToF
arguments: none
returns: none
*/
void ToF_calibrate(void)
{
//magnitude calibration: no user setup is needed
Serial.println("Starting magnitude calibration... You have 5 sec to prepare the device"); //display a message
Serial.println("No user setup is needed"); //display a message
delay(5000); //wait 5s
ToF_calibrate_magnitude(); //performe magnitude calibration

//crosstalk calibration: block all light to the PD
Serial.println("Starting crosstalk calibration... You have 10 sec to prepare the device"); //display a message
Serial.println("Block all light towards the photodiode"); //display a message
delay(10000); //wait 10s
ToF_calibrate_crosstalk(); //performe crosstalk calibration

//distance calibration: mount the board to a known distance from the target
Serial.println("Starting distance calibration... You have 10 sec to prepare the device"); //display a message
Serial.println("Mount the Pmod to a known distance from the target"); //display a message
delay(10000); //wait 10s
ToF_calibrate_distance(CALIBRATION_DISTANCE); //perform distance calibration

//save calibration values in EEPROM
Serial.println("Saving calibration data"); //display a message
EEPROM_write(EEPROM_user); //savevalues in EEPROM
return;
}

/*------------------------------------------------------------------------*/

/*
calibrates the signal magnitude, no user setup is needed
arguments: none
returns: none
*/
void ToF_calibrate_magnitude(void)
{
//save interrupt control settings
unsigned char interrupt_ctrl = read_reg(0x60); //save register value
//save measurement settings
unsigned char measurement_mode = read_reg(0x13); //save register value

ToF_start(); //initiate a measurement
while (digitalRead(IRQ) != 0)
; //wait for data

//read-write magnitude exponent
write_reg(cali_registers[8], read_reg(0xF6)); //load new register with read value
//read-write magnitude MSB
write_reg(cali_registers[9], read_reg(0xF7)); //load new register with read value
//read-write magnitude LSB
write_reg(cali_registers[10], read_reg(0xF8)); //load new register with read value

//restore settings
write_reg(0x60, interrupt_ctrl); //restore interrupt settings
write_reg(0x13, measurement_mode); //restore measurement settings
return;
}

/*------------------------------------------------------------------------*/

/*
calibrates the signal crosstalk, block all light towards the photodiode
arguments: avg_nr - nr of measurements to average (default is 100)
returns: none
*/
void ToF_calibrate_crosstalk(unsigned int avg_nr)
{
//save interrupt control settings
unsigned char interrupt_ctrl = read_reg(0x60); //save register value
//save measurement settings
unsigned char measurement_mode = read_reg(0x13); //save register value

//average measured data
double I = 0, Q = 0, G = 0; //variables for measured data
unsigned char exp, msb, lsb; //variables to read register into
for (int i = 0; i < avg_nr; i++)
{
ToF_start(); //initiate a measurement
while (digitalRead(IRQ) != 0)
; //wait for data

exp += read_reg(0xDA); //get exponent
msb += read_reg(0xDB); //get MSB
lsb += read_reg(0xDC); //get LSB
I += bytes2double(exp, msb, lsb); //add current values to the sum

exp += read_reg(0xDD); //get exponent
msb += read_reg(0xDE); //get MSB
lsb += read_reg(0xDF); //get LSB
Q += bytes2double(exp, msb, lsb); //add current values to the sum

msb += read_reg(0xE6); //get MSB
lsb += read_reg(0xE7); //get LSB
G += ((msb << 8) | lsb); //add current values to the sum
}
I /= avg_nr; //average
Q /= avg_nr; //average
G /= avg_nr; //average

unsigned char measured[13]; //array for measurements
double2bytes(I, &measured[0], &measured[1], &measured[2]); //get first 3 values
double2bytes(Q, &measured[3], &measured[4], &measured[5]); //get second 3 values
measured[6] = ((int)G & 0xFF00) >> 8; //get gain msb
measured[7] = (int)G & 0xFF; //get gain lsb

for (int i = 0; i < 8; i++)
{
measured[i] &= 0xFF; //truncate them if necessary
write_reg(cali_registers[i], measured[i]); //load registers
}

//restore settings
write_reg(0x60, interrupt_ctrl); //restore interrupt settings
write_reg(0x13, measurement_mode); //restore measurement settings
return;
}

/*------------------------------------------------------------------------*/

/*
calibrates the distance offset, mount the Pmod to a known distance from the target
arguments: reference_distance - the reference distance in cm, avg_nr - nr of measurements to average (default is 100)
returns: none
*/
void ToF_calibrate_distance(unsigned int reference_distance, unsigned int avg_nr)
{
//save interrupt control settings
unsigned char interrupt_ctrl = read_reg(0x60); //save register value
//save measurement settings
unsigned char measurement_mode = read_reg(0x13); //save register value

int avg = 0; //variable for averaging
unsigned char MSB, LSB; //variables for data bytes
for (int i = 0; i < avg_nr; i++)
{
ToF_start(); //initiate a measurement
while (digitalRead(IRQ) != 0)
; //wait for data

MSB = read_reg(0xD8); //get phase MSB
LSB = read_reg(0xD9); //get phase LSB
avg += ((int)MSB * 256) + (int)LSB; //add converted nr to sum
}
avg /= avg_nr; //calculate average

//calculate the distance
float distance = (float)avg - ((float)reference_distance * 1967.45722);

MSB = ((unsigned int)distance & 0xFF00) >> 8; //get msb
LSB = (unsigned int)distance & 0x00FF; //get lsb
write_reg(cali_registers[11], MSB); //load MSB
write_reg(cali_registers[12], LSB); //load LSB

//restore settings
write_reg(0x60, interrupt_ctrl); //restore interrupt settings
write_reg(0x13, measurement_mode); //restore measurement settings
return;
}

/*------------------------------------------------------------------------*/

/*
read a register
arguments: reg - register address
returns: register value
*/
unsigned char read_reg(unsigned char reg)
{
unsigned char val = 0x00; //variable for values
Wire.beginTransmission(i2c_address); //add the address to the buffer
Wire.write(reg); //append register address
Wire.endTransmission(); //send buffer
Wire.requestFrom(i2c_address, 1); //request 1 byte of data
if (Wire.available()) //if data is available
{
val = Wire.read(); //read data byte
}
return val;
}

/*------------------------------------------------------------------------*/

/*
write a register
arguments: reg - register address, val - register value
returns: none
*/
void write_reg(unsigned char reg, unsigned char val)
{
Wire.beginTransmission(i2c_address); //add the address to the buffer
Wire.write(reg); //append register address
Wire.write(val); //set register state
Wire.endTransmission(); //send buffer
return;
}

/*------------------------------------------------------------------------*/

/*
convert a double to three bytes
arguments: nr - double, exp - exponent, msb - mantissa msb, lsb - mantissa lsb
returns: none
*/
void double2bytes(double nr, unsigned char *exp, unsigned char *msb, unsigned char *lsb)
{
bool negative = false; //check negativity
if (nr < 0)
{
negative = true; //store flag
nr = -nr; //calculate absolute value
}

int e;
double mantissa = frexp(nr, &e); //get the exponent
*exp = e & 0xFF; //save the exponent
for (int i = 0; i < 15; i++)
{
mantissa *= 2; //shift the mantissa 14 places to the left
}

if (negative)
{
mantissa = -mantissa; //make it negative
}

*msb = ((int)mantissa & 0xFF00) >> 8; //save msb
*lsb = (int)mantissa & 0x00FF; //save lsb
return;
}

/*------------------------------------------------------------------------*/

/*
convert three bytes to double
arguments: exp - exponent, msb - mantissa msb, lsb - mantissa lsb
returns: the converted number
*/
double bytes2double(unsigned char exp, unsigned char msb, unsigned char lsb)
{
bool negative = false; //flag to signal negativity
if (msb > 127) //check if the number is negative or not
{
negative = true; // negative number
}

int mantissa = msb << 8; //recreate mantissa
mantissa |= lsb; //append lsb

double result = 0; //variable to store the result
if (negative)
{
mantissa = ((mantissa - 1) ^ 0xFFFF); // convert from 2's complement
result = -mantissa * pow(2, exp); // combine mantissa and exponent
}
else
{
result = mantissa * pow(2, exp); // combine mantissa and exponent
}

return result; //return the result
}

/*------------------------------------------------------------------------*/

/*
displays all registers in the Serial Monitor
arguments: none
returns: none
*/
void debug(void)
{
Serial.println('\n'); //leave a line out
char str[5]; //string for output data

//control, settings and status registers
Serial.println("control, settings and status registers:"); //print message
for (int i = 0x00; i <= 0x02; i++)
{
sprintf(str, "0x%2X", i); //format data
Serial.print(str); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(i)); //format data
Serial.println(str); //print register value
}

//sampling control registers
Serial.println("sampling control registers:"); //print message
for (int i = 0x10; i <= 0x13; i++)
{
sprintf(str, "0x%2X", i); //format data
Serial.print(str); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(i)); //format data
Serial.println(str); //print register value
}
Serial.print("0x19"); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(0x19)); //format data
Serial.println(str); //print register value

//closed loop calibration registers
Serial.println("closed loop calibration registers:"); //print message
for (int i = 0x24; i <= 0x30; i++)
{
sprintf(str, "0x%2X", i); //format data
Serial.print(str); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(i)); //format data
Serial.println(str); //print register value
}

//ambient light and temperature correction registers
Serial.println("ambient light and temperature correction registers:"); //print message
for (int i = 0x31; i <= 0x30; i++)
{
if (i == 0x31 || i == 0x33 || i == 0x34 || i == 0x36 || i == 0x39 || i == 0x3B) //only valid registers
{
sprintf(str, "0x%2X", i); //format data
Serial.print(str); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(i)); //format data
Serial.println(str); //print register value
}
}

//interrupt registers
Serial.println("interrupt registers:"); //print message
Serial.print("0x60"); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(0x60)); //format data
Serial.println(str); //print register value

//analog control registers
Serial.println("analog control registers:"); //print message
for (int i = 0x90; i <= 0x93; i++)
{
sprintf(str, "0x%2X", i); //format data
Serial.print(str); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(i)); //format data
Serial.println(str); //print register value
}
Serial.print("0xA5"); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(0xA5)); //format data
Serial.println(str); //print register value
Serial.print("0xB0"); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(0xB0)); //format data
Serial.println(str); //print register value

//output registers
Serial.println("output registers:"); //print message
for (int i = 0xD1; i <= 0xE7; i++)
{
sprintf(str, "0x%2X", i); //format data
Serial.print(str); //print register address
Serial.print("\t-\t"); //print separator
sprintf(str, "0x%2X", read_reg(i)); //format data
Serial.println(str); //print register value
}

Serial.println('\n'); //leave a line out
return;
}

/*------------------------------------------------------------------------*/

/*
read data from EEPROM to cali_values array
arguments: address - starting address
returns: none
*/
void EEPROM_read(unsigned char address)
{
Wire.beginTransmission(i2c_EEPROM); //add the address to the buffer
Wire.write(address + 1); //append data address
Wire.endTransmission(); //send buffer

for (int i = 0; i < 13; i++) //repeat for all bytes
{
Wire.requestFrom(i2c_EEPROM, 1); //request 1 byte
if (Wire.available()) //if data is available
{
write_reg(cali_registers[i], Wire.read()); //read and save data byte
}
}
return;
}

/*------------------------------------------------------------------------*/

/*
write data to EEPROM from cali_values array
arguments: address - starting address
returns: none
*/
void EEPROM_write(unsigned char address)
{
unsigned char data[13]; //array to store register values
for (int i = 0; i < 13; i++) //read all registers
{
data[i] = read_reg(cali_registers[i]); //read calibration register value
}

Wire.beginTransmission(i2c_EEPROM); //add the address to the buffer
Wire.write(address + 1); //append data address
for (int i = 0; i < 13; i++) //go through the data array
{
Wire.write(data[i]); //append data byte
}
Wire.endTransmission(); //send buffer
return;
}

Mfr varenr. A000062
ARDUINO DUE ATSAM3X8E EVAL BRD
Arduino
313,20 kr.
View More Details
Mfr varenr. 410-392
PMOD TOF: TIME OF FLIGHT SENSOR
Digilent, Inc.
126,74 kr.
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.