HUBER+SUHNER Brings Unmatched Performance and Value to Test & Measurement Applications

It’s common for significant time and money to be spent on defining products for a high performance analog or digital test station. One needs to source the right network analyzer, oscilloscope, bit-error-rate tester or other expensive equipment trying to ensure high fidelity test results. Conversely, all too often the microwave cables which connect these various pieces of equipment to the device under test (DUT) are taken as an after-thought and lead to limited performance of the integrated system.

At HUBER+SUHNER, we offer a broad range of microwave cables with superior electrical and mechanical performance. In today’s business conditions, performance is only one important factor to consider when evaluating your microwave cable partner. In the test environment, it’s also critical to be able to source cables as close to real time as possible, avoiding costly project delays. Meanwhile, other stakeholders in the organization might be most concerned with unit costs aligning with a set budget. All three factors must be considered concurrently.

(Image source: HUBER+SUHNER)

Our Sucoflex™ family of cables are available with various connector interfaces offering bandwidth from DC to 110 GHz. Too numerous to list here in total, options include N, SMA, 2.92 mm, 2.4 mm, 1.85 mm and 1.0 mm interfaces. Cables can be supplied with integrated armoring constructions or without based on the needs of the application. Fully terminated assemblies are available in select configurations or customized assemblies where custom lengths are required. For electrical phase and delay sensitive testing protocols, cable assemblies are available in matched condition. All Sucoflex cables are delivered with factory test results giving the user confidence upon installation. Further, production at scale in several global HUBER+SUHNER facilities supports a lower cost for our partners as well as flexibility in planning thereby ensuring low lead time.

Additionally, within the Sucoflex™ cable family, HUBER+SUHNER utilizes a rotary swaging process applied to the center conductor of select cables, thereby differentiating performance in the market. You don’t have to choose between stability, over flexure, or loss performance. You CAN have it all.

Taking into account all of the value the Sucoflex™ family of cables offers, it is clear that choosing HUBER+SUHNER as your partner for high performance test leads will offer the best combination of performance, price and delivery.

Furthermore, as a trusted partner to HUBER+SUHNER, DigiKey offers Sucoflex solutions off-the-shelf to allow you even less down time due to test cycles.

Additional Links and Resources:

DigiKey | HUBER+SUHNER | Sucoflex_500 listing

SUCOFLEX 500 - Huber+Suhner | DigiKey

SUCOFLEX 500 Catalogue - Huber+Suhner | DigiKey

SUCOFLEX 500 Family Combines Low Loss High Flexibility - Huber+Suhner | DigiKey

HUBER + SUHNER Test and Measurement video

Om denne forfatter

Image of HUBER+SUHNER

Huber+Suhner offers their customers around the globe outstanding products and services for their electrical and optical connectivity needs. Their focus is on the three main markets of industrial, communication, and transportation, which are addressed with applications from the three technologies of radio frequency, fiber optics, and low frequency.

Huber+Suhner products deliver high performance, quality, reliability, and long service life – even under the toughest conditions. A global production network, combined with subsidiaries and agencies in over 80 countries, puts Huber+Suhner close to its customers.

More posts by HUBER SUHNER
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum