How to Synchronize Pneumatic Components for Maximum Efficiency
Bidraget af DigiKeys nordamerikanske redaktører
2026-01-29
In industrial automation, efficiency is often treated as a component-level specification. Engineers may select a high-efficiency actuator or a low-wattage valve and assume the system will operate efficiently. However, machines built with efficient parts can still consume excess energy if those components are not synchronized.
Energy loss in pneumatics is often due to system architecture rather than individual component failure. An efficient actuator cannot perform optimally if fed by restricted tubing or controlled by an oversized valve. Therefore, energy savings are achieved by harmonizing the entire pneumatic chain to minimize restrictions and dead volume at every interface. This article outlines a system-level approach to pneumatic design, demonstrating how synchronizing six key component categories can improve energy efficiency.
Reducing the initial pressure drop through better preparation
System efficiency begins at the air preparation stage. Undersized or clogged air preparation units can create a pressure drop. If a filter regulator causes a pressure drop due to flow restriction, the compressor must operate at a higher pressure to overcome that resistance. Such a move results in energy being used solely to push air through a restriction rather than to move the load.
The first step in a synchronized system is a high-flow air preparation unit. The MS Series Filter Regulator (MS6-LFR) from Festo, shown in Figure 1, is designed to minimize this initial restriction. With a normal nominal flow rate of 4000 l/min (normalized to DIN 1343), the MS6-LFR maintains a consistent supply to downstream components, even during peak demand.
Figure 1: The MS6-LFR filter regulator combines high-flow filtration (4000 l/min) with precise pressure regulation to eliminate inlet bottlenecks. (Image source: Festo)
The regulator also features a regulation range of 0.5 bar to 12 bar, allowing the machine's base pressure to be set to the exact level required. For the same purpose, the LRP precision regulator (Figure 2) offers a maximum pressure hysteresis of 0.02 bar for applications requiring high stability, ensuring consistent system pressure.
Figure 2: The LRP-1/4-4 precision regulator features 0.02 bar hysteresis for ultra-stable pressure control in sensitive applications. (Image source: Festo)
Both regulators also include secondary exhausting. If downstream pressure increases (e.g., due to external forces on an actuator), the regulator vents the excess pressure, preventing backpressure that opposes motion. Using a regulator that provides a consistent flow keeps main line pressure at the minimum necessary level, reducing overall energy usage.
Optimizing energy with point-of-use regulation
Many systems supply the entire machine at the pressure required by its single most demanding actuator. For example, if a heavy press requires 6 bar, the entire circuit is often pressurized to 6 bar, even for lightweight clamping or return strokes that only require 3 bar. This wastes nearly 50% of the energy for those lighter tasks.
Decentralized regulation involves creating pressure zones directly at the point of use with the MS2-LR pressure regulator, shown in Figure 3. The regulator is compact (Size 2) and handles flow rates up to 350 l/min, making it ideal for isolating specific machine clusters. In other words, installing an MS2-LR locally can supply the main manifold at 6 bar but regulate a specific branch down to 3 bar for lighter tasks.
Figure 3: The MS2-LR pressure regulator brings pressure control directly to the actuator. (Image source: Festo)
Unlike basic regulators, the MS2-LR includes a return flow function and secondary exhausting. This ensures that excess pressure can be rapidly exhausted during the return stroke or during system venting, preventing pneumatic locking and ensuring safety.
The MS2-LR-QS6-D6-AR-BAR-B model (Figure 4) includes an integrated pressure gauge, allowing operators to visually verify that the zone is operating at its reduced, energy-efficient setting. On the other hand, for even lighter weight (28.3 g), the A8 variant offers a prepared port for custom gauging.
Figure 4: Integrated monitoring enables instant verification of energy-saving pressure zones. (Image source: Festo)
Minimizing dead volume in air transmission
Tubing between the valve and the actuator is a significant source of energy loss. The volume within the tubing must be pressurized and depressurized with every cycle. This dead volume consumes compressed air without performing work. Additionally, leaks in tubing increase the compressor's base load.
Transmission efficiency is achieved through material selection and geometric optimization.
- Material Integrity: PUN-H Tubing is manufactured from hydrolysis-resistant TPE-U (polyurethane). Unlike standard PVC, which may degrade and leak over time, PUN-H maintains flexibility and seal integrity in various environments, with an operating temperature range of -35°C to +63°C. Its smooth inner wall minimizes friction, promoting laminar flow.
- Geometry Strategy: Placing valves closer to actuators and connecting them with cut-to-length tubing reduces the volume of air required per cycle. The PUN-H series enables circuit identification through color coding, with the Black and Blue variants offering a superior minimum bending radius of 9.7 mm for tight routing. Note that the natural color variant has a slightly larger bending radius (14 mm), so the product selection should be matched to the available installation space.
Optimizing valve selection for energy efficiency
Valves are sometimes selected based on port size rather than flow characteristics. Oversized valves supply excessive air volume to small cylinders, leading to inefficiency. Conversely, a restrictive valve slows the actuator, prompting operators to increase pressure to compensate. The valve should balance speed with consumption.
The VUVG solenoid valve, shown in Figure 5, is engineered for this purpose.
- Flow-to-Size Ratio: The VUVG provides a high flow rate (e.g., 660 l/min for the 14 mm size) in a compact design, driving loads without creating a restriction.
- Speed & Precision: With a changeover time of 8 ms (for the bistable variant) and a max switching frequency of 2 Hz, the VUVG provides fast response. As such, this precision helps prevent line over pressurization caused by delayed valve closure.
- Low Power Consumption: The VUVG coil consumes 0.8 W (at 24 V DC). Combined with an IP65 protection rating, it ensures reliability in industrial environments without drawing excess current.
Figure 5: The VUVG solenoid valve’s high flow-to-size ratio ensures the VUVG drives loads without restriction. (Image source: Festo)
Selecting a valve matched to the actuator's volume ensures the cylinder receives the necessary air volume without waste.
Reducing energy load with lighter actuators
Heavier moving parts require more force (and pressure) to move. Hence, using an oversized cylinder increases the energy needed for acceleration, contrary to the principle of reducing weight. Furthermore, every millimeter of unnecessary bore size increases the volume of air required to fill the cylinder, which leads to compounding energy waste on every stroke, regardless of the actual load being moved. The actuator should be optimized for the application.
The DSBC ISO Cylinder is designed for performance with reduced mass. Figure 6 shows DSBC-32-25-PPVA featuring a moving mass of 133 g. It delivers a theoretical advancing force of 483 N at 6 bar. This power-to-weight ratio reduces the force required to accelerate the piston compared to heavier alternatives.
Figure 6: The DSBC ISO cylinder combines low moving mass with effective cushioning to maximize kinetic energy usage. (Image source: Festo)
The DSBC family features pneumatic cushioning options that improve efficiency. The DSBC-32-25-PPVA features adjustable cushioning with a 17 mm length to smoothly decelerate the load (impact energy < 0.4 J). For even greater simplicity, the DSBC also offers a self-adjusting variant (PPSA) that eliminates the need for manual adjustment screws, reducing maintenance and the risk of leaks.
Minimizing friction in guided motion
In precision applications, friction reduces efficiency. Standard sliding guides create drag, requiring higher air pressure to overcome static friction and maintain motion. This opposes the goal of lowering friction. Over time, wear at sliding contact points can degrade positioning accuracy and create inconsistent resistance, forcing the system to work harder to maintain speed.
For guided tasks, the DGST-10-20-E1A mini slide (Figure 7) utilizes rolling elements to improve efficiency.
- Recirculating Ball Bearings: The DGST carriage uses a precision ball bearing guide instead of sliding bushings. Such a move lowers the coefficient of friction, enabling smooth operation at speeds up to 0.5 m/s.
- Twin Piston Efficiency: The twin-piston design increases force output in a compact unit. The slide delivers 94 N of theoretical force (advancing at 6 bar) with a moving mass of 134 g.
- Integrated Yoke: Integrating the slide and yoke into a rigid unit eliminates misalignment. The unit handles loads with a maximum torque of 3 Nm and a maximum force of 480 N, converting air pressure directly into linear motion.
Figure 7: The DGST mini slide uses recirculating ball bearings to reduce friction, drastically outperforming sliding guides. (Image source: Festo)
Conclusion
Optimizing a pneumatic system requires an architectural approach rather than a single component change. By viewing the system as a synchronized chain, engineers can achieve cumulative efficiency gains that far exceed individual part upgrades. When these six elements mentioned in the article are harmonized, efficiency can be improved, pressure can be lowered, cycle times can be reduced, and leaks can be minimized. This phenomenon thereby strengthens component connections and enhances overall performance.
Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.