• Preferred Supplier

Amgis

Seneste PTM’er

Image of Amgis' Thor and Hercules Converters
5 minutes
Thor and Hercules Converters
This presentation will introduce the features and applications for the Thor and Hercules converters from Amgis.
LM2594 Inductor
10 minutes
Inductor selection for LM2594
The process for selecting the appropriate inductor when designing a continuous mode buck converter using the LM2594 or LM2597 series switching regulator.
LM2595 Inductor
5 minutes
Inductor selection for LM2595
The process for selecting the appropriate inductor when designing a continuous mode buck converter using the TI LM2595 series switching regulator.
MED Series Power Transformer
5 minutes
MED Series Medical Transformers
Toroidal transformers are compact, low weight, highly efficient, have low stray magnetic field, and are specifically for medical applications.
Vis alle

Om Amgis

Amgis is a manufacturer/importer of high frequency inductive components and AC/DC power supplies. We import and export components daily through our purchasing and sales networking systems, including India, Asia, Europe, and the United States. The majority of our standard components are manufactured at our ISO9001 certified facility located in Salem, India. Our strength is in our service, having qualified engineers at all of our locations, and exceptional customer service teams, we can qualify most requirements and have answers to requests within hours instead of days.

Amgis was originally a subsidiary of the Talema Group and carries all the Talema high frequency component lines, including power inductors, common mode chokes, current sensors, telecom products, and networking products. Also, we have diversified into the switching power supply market, including standard lines and custom designs, both open style and enclosed. By drawing upon the resources of our extensive worldwide network, Amgis provides its customers with high quality components at very competitive prices.