Protect Your SMD Power Product from Damaging Moisture

When it comes to mounting components to circuit boards, surface mount technology saves board space and assembly time. Advantages include higher component density, resulting in smaller circuits and faster circuit speeds, plus shock and vibration resistance, and low noise. Because of these and other benefits, surface mount-packaged (SMD) components are a logical choice for automated assembly. However, moisture can cause a “popcorn effect” during solder reflow.

To help OEMs take proper care when handling and storing moisture-sensitive devices, the Association Connecting Electronic Industries created the IPC-M-109 Moisture-sensitive Component Standards and Guideline Manual. Among its seven documents, IPC-M-109 defines moisture sensitivity levels (MSLs), with each numerical level corresponding to the part’s risk of incurring the popcorn effect. Level 1 is the lowest risk while Level 6 indicates the highest risk. Each level determines how long a moisture-sensitive device can be exposed to ambient room conditions (≤30°C and 85 percent relative humidity at Level 1; all other levels: ≤30°C and 60 percent relative humidity).

The MTWA4 Series low-power DC-DC converters feature a compact size and 4.5 to 12V DC input voltage range, making them well-suited for portable medical devices. (Image source: Daburn Electronics' Polytron Devices Division)

Find out the Product’s Floor Life

Many vendors list MSL information under the “Environmental” section of the datasheet. For example, the datasheet for Daburn Electronics' Polytron Devices MTWA4 Series of 3.5 W DC-DC converters for medical applications indicates they are available in a 0.95 x 0.57 x 0.40-inch miniature SMD package and carry an MSL level of 2. That means it can be stored, mounted, and reflowed within one year of “floor life” outside of a moisture barrier bag at less than or equal to 30°C and 60 percent relative humidity. Should the part exceed its floor life, that moisture will have to be baked out, slowly, before assembly. In addition to their miniature size, the MTWA4 converters provide 5,000 VAC input to output 2 MOPP isolation and remote ON/OFF. Their voltage input range (4.5 to 12V DC) makes them well-suited for portable devices. The MTWA4 Series of SMD-packaged DC-DC converters are well-suited for automated assembly and can satisfy various input and output requirements.

When using a surface mount component in your design, manufacturability and reliability depend on proper storage. Be sure to check the manufacturer’s datasheet for the part’s numerical moisture sensitivity level (MSL) to determine its floor life, and to refer to IPC J-STD-020 and J-STD-033 for other storage and handling procedures based on the MSL. The better informed you are about moisture levels according to JEDEC/IPC standards, you’ll have more certainty that your part will perform as intended.

To learn more, get in touch with our technical staff.

Om denne forfatter

Image of Sheri Lynn (Daburn)

Sheri Lynn, Director of sales for the power supply division of Daburn Electronics, has been with the company for 1.5 years. Prior to that, she was the International Sales manager of Polytron Devices, a leading manufacturer of Power Supplies and DC/DC Converters. Sheri has a science background with a BS degree from Rutgers University and over 29 years of power supply experience. She has worked her way up in varying roles including assembly, technical sales assistant, assistant marketing manager, technical writer and international sales manager. When not finding solutions to world wide power supply requirements, her free time is spent finding solutions to life’s daily issues as well as listening to music, swimming, trying out new restaurants, and laughing with friends and family.

More posts by Sheri Lynn
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum