Creating Your Own PLC with STMicroelectronics

The STMicroelectronics X-NUCLEO-OUT01A1 is an expansion board that features ST's ISO8200BQ galvanic 8-channel high power relay. When used with the Nucleo PLC board (X-NUCLEO-PLC01A1), an appropriate STM32 Nucleo development board (NUCLEO-F103RB, NUCLEO-F302R8 and NUCLEO-F401RE), and a wireless shield (X-NUCLEO-IDW01M1), the result is an 8 input/16 0.5 A output industrial PLC with IoT connectivity. This solution gives engineers a head-start in creating a design that utilizes connectivity as well as power without actually using a PLC. For more information including quick start guides, schematics, and software downloads, check out the STMicroelectronics landing page for the X-NUCLEO-OUT01A1.

Photo from last page of STMicroelectronics' X-NUCLEO-OUT01A1 Quick Start Guide

Om denne forfatter

Image of Linzee Loerzel

Linzee Loerzel, Partnership Marketing Manager, has been with DigiKey since 2005 helping supplier partners showcase products to the engineering community. She holds degrees in Electronics Technology Automated Systems and Electronic Component Marketing and is working toward another degree in Marketing Communication. In her free time, Linzee enjoys piano lessons and volunteering as a Minnesota Master Gardener.

More posts by Linzee Loerzel
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum