It is essential to consider the maximum pressure that can be placed on the components. For example, if a BGA is used, the maximum pressure applied must be minimised. In this case, a proper solution would be to use a softer gap filler or a putty. A putty could be especially effective as it can be compressed by as much as 90% with pressures as low as 2 PSI.