Maker.io main logo

Zipper Switch

46

2023-03-07 | By Adafruit Industries

License: See Original Project Wearables FLORA Gemma

Courtesy of Adafruit

Guide by Becky Stern

Overview

Here’s a fun way to make your clothes more interactive-- you can ‎turn a zipper into a switch for activating lights, sounds, and more ‎using stainless steel conductive thread.‎

 

 

zipper_1

The switch works like a momentary pushbutton. As the zipper pull ‎travels along the teeth, two pads of conductive thread are bridged, ‎momentarily creating an electrical connection.‎

This connection can be sensed by a microcontroller like FLORA or ‎GEMMA with an activated internal pullup resistor or be used in place ‎of a push button in circuits like the TV-B-Gone or audio FX boards.‎

The zipper switch is not delivering current and should not be used to ‎drive LEDs-- it's a very weak connection that is only made ‎momentarily and not suitable for more than a few milliamps of ‎current.‎

metal_2

Find a metal zipper pull, not plastic. If it’s painted, use some ‎sandpaper to sand it off.‎

find_3

The teeth of the zipper can be plastic or nylon, so long as the zipper ‎pull is metal!‎

Stitch long strands

stitch_4

Use straights stitches to bring two long pieces of conductive thread ‎to the edge of the zipper.‎

sew_5

You can put 2-ply thread in the bobbin of your sewing machine, then ‎pick up long tails with a needle and hand-stitch the rest.‎

Stitch pads near zipper

pads_6

Build up stitches to make two small pads of thread. They should be ‎close enough together that when the pull goes by, it briefly touches ‎both pads at once.‎

build_7

You want the knots away from the zipper, so stitch a bit back and tie ‎off, then seal with a dab of clear nail polish. Let it dry before cutting ‎the thread short.‎

polish_8

Attach to circuit

attach_9

At the other ends of the thread, stitch one to ground and the other to ‎a digital input on your FLORA or GEMMA microcontroller.‎

ends_10

Don’t forget to activate the internal pull up resistor when you set up ‎your Arduino sketch.‎

‎Download File‎

Copy Code
void setup(){
  pinMode(1, INPUT_PULLUP);

}

Use it!‎

use_11

It acts like a momentary switch. You can use a zipper switch in place ‎of a pushbutton, like in this TV-B-Gone jacket.‎

push_12

I stitched this a few years ago with silver conductive thread, and it’s ‎tarnished. That’s why we carry only stainless-steel thread! It’s a little ‎more expensive but will last a lot longer.‎

Mfr Part # 641
THREAD 316L THIN COND 3PLY 60'
Adafruit Industries LLC
64,18 kr.
View More Details
Mfr Part # 615
NEEDLE SET SIZE 3-9 20PC
Adafruit Industries LLC
12,48 kr.
View More Details
Mfr Part # 659
FLORA ELECTRONIC PLATFORM V3
Adafruit Industries LLC
95,68 kr.
View More Details
Mfr Part # 1222
WEARABLE PLATFORM GEMMA V2 MINI
Adafruit Industries LLC
64,18 kr.
View More Details
Mfr Part # 73
TV-B-GONE KIT UNIVERSAL V1.2
Adafruit Industries LLC
124,80 kr.
View More Details
ESD-SAFE PCB CLEANING BRUSH
Mfr Part # 1209
ESD-SAFE PCB CLEANING BRUSH
Adafruit Industries LLC
18,88 kr.
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.