Maker.io main logo

EL Wire Hoodie

38

2018-11-15 | By SparkFun Electronics

License: See Original Project Wearables

Courtesy of SparkFun

Introduction

The design and build time of this project depends on your experience manually sewing, the length of EL wire used, and where you are sewing it to. This can take about ~1 - 3 hours if you are following the edges of a hoodie.

Heads up! The hoodie that was used in this tutorial was a youth medium sized hoodie with standard EL wire sewn around the front, hood, and shoulders. The length of wire used was 3 meters. Depending on the size of the hoodie, you may end up needing more or less EL wire as explained further below. Make sure to plan accordingly.

In this tutorial, we will sew standard EL wire onto a hoodie.

Figure 1

Required Materials

To follow along with this tutorial, you will need the following materials. We will be using a standard EL wire on the hoodie. You may not need everything, depending on what you have and your setup. Add it to your cart, read through the guide, and adjust the cart as necessary.

Note: EL comes in many different colors. 

Looking for EL chasing or bendable EL wire?

Tools

At a minimum, you will need a needle. If you are making an extension cable, you will need a soldering iron, solder, and general soldering accessories.

  • Needle Set

You Will Also Need

  • Hoodie

  • Clear Thread or Fishing Line

  • Binder Clips, Pins, or, Tape

  • Scissors

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

Prepare the EL Wire

Note: The images below is using standard EL wire with a youth medium sized hoodie. The length of wire used was 3 meters. Depending on the size of the hoodie, you may end up needing more or less EL wire as explained further below. Make sure to plan accordingly.

Testing the EL Wire and EL Inverter

Before sewing the EL wire to a piece of clothing, make sure to test it out to see if it is functioning. To test, connect the EL wire to an inverter. In this case, we are using AA batteries and the 3V EL inverter battery pack.

Figure 2

With the battery in the EL inverter battery pack, press the button to test. If the EL wire lights up, both the EL wire and EL inverter are good to go!

Figure 3

Planning the Path

Plan out where to add EL wire. While you can sew the EL wire on the arms, it will be harder due to the amount of room available to work with in the arm. The easiest would be to follow the edge of the hoodie. To hold down the EL wire when sewing, we will be using binder clips. Depending on what you have, you could also try to use pins or tape. Place the EL wire into the binder clip and clamp it down against on the fabric. Make sure to avoid clamping the EL wire down where the binder clip pinches as this can damage the corona wires.

Figure 4

In this case, all 3 meters were used for EL wire starting under the pocket, running up the side of the zipper, around the shoulders, up to the brim of the hood, around the shoulders, down the zipper, and ending at the pocket on the other side. Make sure to avoid sharp bends. If you decide to use a shorter length, you can cut the EL wire. Just make sure to re-seal the cut end with hot glue, otherwise you could end up getting a good jolt..

Figure 5

Having a hard time seeing the binder clips and EL wire? 

Heads up! Loose fabric like cotton can be harder to sew unless you have a something to hold the thread down.

Prepare the Needle and Thread

For this tutorial, we will double up the clear thread. Prepare your needle and thread by inserting the end of the clear thread through the eye (opening) of the needle and pull it through. Cut about an arms length of thread (approximately 2 feet long) to work with. Tie the two ends of the fishing wires into a knot. You may need to use the needle to help guide the knot close to the end of the thread.

Figure 6

Repeat the steps again for a second knot. Cut of any excess tail left over.

Figure 7

Tip: The clear thread is non-conductive. However, try checking out the section on sewing with conductive thread for other alternatives to start a knot.

Sewing EL Wire

Heads up! The hoodie that was used in this tutorial was a youth medium sized hoodie with standard EL wire sewn around the front, hood, and shoulders. The length of wire used was 3 meters. Depending on the size of the hoodie, you may end up needing more or less EL wire as explained further below. Make sure to plan accordingly.

Please note: While sewing, make sure that your EL wire is disconnected from power. Also, make sure what while sewing you do not stab yourself or the EL wire.

Start sewing at the EL wire’s heat shrink and tie a knot around the EL wire. Continue making a loop around the EL wire to hold it down. When sewing with clear thread, make sure to pull the thread all the way through since the thread is slippery when sewn in certain fabrics. Be careful not to sew the front and back of the hoodie together. Also, ensure that the distance between each stitch is not too long. About 0.5" to 1.0" is a good stitch. Longer stitches can cause the EL wire to snag or become loose when wearing the EL hoodie.

Figure 8

After about 5x stitches, loop back through the last stitch with a overhand knot to lock the thread in and prevent it from sliding.

Figure 9

Continue sewing and remove any binder clips holding the EL wire down against the fabric. When sewing EL along the zipper, avoid looping the thread against the zipper.

Figure 10

While sewing the EL wire, try holding the EL down against the fabric using your non-dominant hand. Pinch below the area that you are sewing using your thumb and ring finger. Then pinch above the area that you are sewing using your index and middle finger. This keeps the center area (where you will be working with the needle) taut so that it is easier to sew.

Figure 11

Once you begin to run out of thread to work with, tie the clear thread down against the fabric. Then repeat the steps outlined above with another piece of clear thread.

Figure 12

When you are finished sewing the EL wire down, make a loop with the end of the EL wire cable and sew the wire down for strain relief. Make sure this loop is in the wiring beyond the heat shrink, as the connection at the heat shrink is sensitive to bending.

Figure 13

Plug the EL wire back into the EL inverter to test it out. If it lights up, you are good to go! Place the EL inverter in a pocket or clip to a belt to enjoy!

Figure 14

Remember, EL wire works best in low light. It may be hard to see in daylight or in rooms with sources of light.

Figure 15

Figure 16

Different Hoodie Sizes

Remember what I said about the size of the hoodie? Different hoodie sizes will require different lengths of EL wire - this variation can cause the EL wire to not start or end where you expect it to. Note the difference in the image in the bottom right.

Figure 17

Sewing Into The Arms

Looking for a challenge? Sewing EL wire onto the arms can be difficult depending on the fabric being used and the amount of space you have to work with. Three pieces of corrugated cardboard were custom cut to fit inside a hoodie’s arm to help with sewing. To assemble, cut half way into the cardboard about 0.5"-1"“ away from the edge. It does not have to be perfect. Slide the cardboard pieces together and hot glue the joints.

Figure 18

Front View of Cardboard Bracket

Trim down the edges as necessary to slide into the arm with ease.

Figure 19

Once cut and assembled, insert the bracket into an arm.

Figure 20

Clamp the fabric material down against the cardboard bracket and ensure that the fabric material is taut. Continue sewing clear thread down/up the arm.

Figure 21

The following shows standard EL wire sewn into the arms of an adult medium hoodie.

Figure 22

Mfr Part # 11222
EL INVERTER - BATTERY PACK
SparkFun Electronics
32,00 kr.
View More Details
Mfr Part # 10197
EL WIRE - WHITE 3M
SparkFun Electronics
63,68 kr.
View More Details
Mfr Part # EN91
BATTERY ALKALINE 1.5V AA
Energizer Battery Company
3,71 kr.
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.