LT1812
L7 LJUW
LT1812
11
1812fb
Layout and Passive Components
The LT1812 amplifi er is more tolerant of less than ideal
layouts than other high speed amplifi ers. For maximum
performance (for example, fast settling) use a ground
plane, short lead lengths and RF-quality bypass capacitors
(0.01μF to 0.1μF). For high drive current applications, use
low ESR bypass capacitors (1μF to 10μF tantalum).
The parallel combination of the feedback resistor and gain
setting resistor on the inverting input combine with the
input capacitance to form a pole that can cause peaking
or even oscillations. If feedback resistors greater than 2k
are used, a parallel capacitor of value
C
F > RG • CIN/RF
should be used to cancel the input pole and optimize
dynamic performance. For applications where the DC
noise gain is 1 and a large feedback resistor is used, CF
should be greater than or equal to CIN. An example would
be an I-to-V converter.
Input Considerations
Each of the LT1812 amplifi er inputs is the base of an NPN
and PNP transistor whose base currents are of opposite
polarity and provide fi rst-order bias current cancellation.
Because of variation in the matching of NPN and PNP
beta, the polarity of the input bias current can be positive
or negative. The offset current does not depend on beta
matching and is well controlled. The use of balanced source
resistance at each input is recommended for applications
where DC accuracy must be maximized. The inputs can
withstand differential input voltages of up to 3V without
damage and need no clamping or source resistance for
protection.
The device should not be used as a comparator because
with sustained differential inputs, excessive power dissi-
pation may result.
Capacitive Loading
The LT1812 is stable with a 1000pF capacitive load,
which is outstanding for a 100MHz amplifi er. This is
accomplished by sensing the load induced output pole
and adding compensation at the amplifi er gain node. As
APPLICATIONS INFORMATION
the capacitive load increases, both the bandwidth and
phase margin decrease so there will be peaking in the
frequency domain and in the transient response. Coaxial
cable can be driven directly, but for best pulse fi delity, a
resistor of value equal to the characteristic impedance of
the cable (i.e., 75Ω) should be placed in series with the
output. The other end of the cable should be terminated
with the same value resistor to ground.
Slew Rate
The slew rate is proportional to the differential input
voltage. Highest slew rates are therefore seen in the lowest
gain confi gurations. For example, a 5V output step in a
gain of 10 has a 0.5V input step, whereas in unity gain
there is a 5V input step. The LT1812 is tested for slew
rate in a gain of –1. Lower slew rates occur in higher
gain confi gurations.
Shutdown
The LT1812 has a shutdown pin (SHDN, Pin 8) for
conserving power. When this pin is open or biased at
least 2V above the negative supply, the part operates
normally. When pulled down to V–, the supply current
drops to about 50μA. Typically, the turn-off delay is
1μs and the turn-on delay 0.5μs. The current out of the
SHDN pin is also typically 50μA. In shutdown mode, the
amplifi er output is not isolated from the inputs, so the
LT1812 shutdown feature cannot be used for multiplexing
applications. The 50μA typical shutdown current is
exclusive of any output (load) current. In order to prevent
load current (and maximize the power savings), either
the load needs to be disconnected, or the input signal
needs to be 0V. Even in shutdown mode, the LT1812 can
still drive signifi cant current into a load. For example, in
an AV = 1 confi guration, when driven with a 1V DC input,
the LT1812 drives 2mA into a 100Ω load. It takes about
500μs for the load current to reach this value.
Power Dissipation
The LT1812 combines high speed and large output drive
in a small package. It is possible to exceed the maximum
junction temperature under certain conditions. Maximum