Tex m 5n nkS/s
Ch}
m M] Dams ch: \
5.16v
Tex-Imomsls
3*
[1559 Azqs
”NWMMJ ~ww~mw _.HM__ .4
ch: vunv WM Surms ch31 4sv
rm : nn v ‘ nn v a
NCP1294
http://onsemi.com
9
of the Soft−Start can be programmed through a capacitance
connected to the SS pin. The constant charging current to the
SS pin is 50 mA (typ).
The VREF (ok) comparator monitors the 3.3 V VREF
output and latches a fault condition if VREF falls below 3.1 V.
The fault condition may also be triggered when the OV pin
voltage rises above 2.0 V or the UV pin voltage falls below
1.0 V. The undervoltage comparator has a built−in hysteresis
of 75 mV (typ). The hysteresis for the OV comparator is
programmable through a resistor connected to the OV pin.
When an OV condition is detected, the overvoltage
hysteresis current of 12.5 mA (typ) is sourced from the pin.
In Figure 6, the fault condition is triggered by pulling the
UV pin to the ground. Immediately, the SS capacitor is
discharged with 5.0 mA of current (typ) and the GATE output
is disabled until the SS voltage reaches the discharge voltage
of 0.3 V (typ). The IC starts the Soft−Start transition again
if the fault condition has recovered as shown in Figure 6.
However, if the fault condition persists, the SS voltage will
stay at 0.1 V until the removal of the fault condition.
Figure 6. The Fault Condition Is Triggered when
the UV Pin Voltage Falls Below 1.0 V. The
Soft−Start Capacitor Is Discharged and the GATE
Output Is Disabled. CH2: Envelop of GATE Output,
CH3: SS Pin with 0.01 mF Capacitor, CH4: UV Pin
Current Sense and Overcurrent Protection
The current can be monitored by the ISENSE pin to achieve
pulse by pulse current limit. Various techniques, such as a
using current sense resistor or current transformer, can be
adopted to derive current signals. The voltage of the ISET pin
sets the threshold for maximum current. As shown in
Figure 7, when the ISENSE pin voltage exceeds the ISET
voltage, the current limit comparator will reset the GATE
latch flip−flop to terminate the GATE pulse.
Figure 7. The GATE Output Is Terminated When
the ISENSE Pin Voltage Reaches the Threshold Set
By the ISET Pin. CH2: ISENSE Pin, CH4: ISET Pin,
CH3: GATE Pin
The current sense signal is prone to leading edge spikes
caused by the switching transition. A RC low−pass filter is
usually applied to the current signals to avoid premature
triggering. However, the low pass filter will inevitably
change the shape of the current pulse and also add cost. The
NCP1294 uses leading edge blanking circuitry that blocks
out the first 150 ns (typ) of each current pulse. This removes
the leading edge spikes without altering the current
waveform. The blanking is disabled during Soft−Start and
when the VCOMP is saturated high so that the minimum
on−time of the controller does not have the additional
blanking period. The max SS detect comparator keeps the
blanking function disabled until SS charges fully. The output
of the max Duty Cycle detector goes high when the error
amplifier output gets saturated high, indicating that the
output voltage has fallen well below its regulation point and
the power supply may be underload stress.
Oscillator and Synchronization
The switching frequency is programmable through a RC
network connected to the RTCT Pin. As shown in Figure 8,
when the RTCT pin reaches 2.0 V, the capacitor is discharged
by a 1.0 mA current source and the Gate signal is disabled.
When the RTCT pin decreases to 1.0 V, the Gate output is
turned on and the discharge current is removed to let the
RTCT pin ramp up. This begins a new switching cycle. The
CT charging time over the switch period sets the maximum
duty cycle clamp which is programmable through the RT
value as shown in the Design Guidelines. At the beginning
of each switching cycle, the SYNC pin generates a 2.5 V,
320 nS (typ) pulse. This pulse can be utilized to synchronize
other power supplies.