VE_—:
wiik‘lH [LKKIRONIK
Cautions and Warnings:
The following conditions apply to all goods within the product series of Thick Film
Resistors of Würth Elektronik eiSos GmbH & Co. KG:
General:
• This electronic component was designed and manufactured for use in general electronic equipment.
• Würth Elektronik must be asked for a written approval (following the certain PPAP level procedure) before incorporating the components
into any equipment in the field such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train
control, ship control), transportation signal, disaster prevention, medical, public information network etc. where higher safety and
reliability are especially required and/or if there is the possibility of direct damage or human injury.
• Electronic components that will be used in safety-critical or high-reliability applications, should be pre-evaluated by the customer.
• Direct mechanical impact to the product shall be prevented as material of the body, pins or termination could flake or in the worst case
it could break.
• Avoid any water or heavy dust on resistor s surface, which may cause electrical leakage, damage, overheating or corrosion.
• Würth Elektronik products are qualified according to international standards, which are listed in each product reliability report. Würth
Elektronik does not warrant any customer qualified product characteristic, beyond Würth Elektronik specifications, for its validity and
sustainability over time.
• The customer is responsible for the functionality of his or her own products. All technical specifications for standard products also apply
to customer specific products.
• The component was designed and manufactured to be used within the datasheet specified values. If the usage and operation conditions
specified in the datasheet are not met, the body, pins or termination may be damaged or dissolved.
• Do not apply any kind of flexural or compressive force onto soldered or unsoldered component.
• The resistance tolerance as specified within the datasheet is only valid on the date of delivery and according specified measurement
criteria.
Product specific:
Storage conditions:
• A storage of Würth Elektronik products for longer than 24 months is not recommended. Within other effects, the terminals may suffer
degradation, resulting in bad solderability. Therefore, all products shall be used within the period of 24 months based on the day of
shipment.
• Do not expose the components into direct sunlight.
• These product must be stored in stable conditions within an ambient temperature between 5°C to 35°C with a relative humidity of 25 to
75%.
• The environment in which the resistors are operated and stored has to have atmospheric characteristics and must be free of dew
condensation and toxic gases (e.g. chlorine, ammonia, sulfur, hydrogen sulphide and hydrogen sulfate).
Operating climatic conditions:
• Do not exceed the lower nor the upper specified temperature under no circumstances.
• Be aware that the specified resistance tolerance is only valid at the date of delivery.
• Do not use the resistors under high humidity, high temperature nor under high or low atmospheric pressure which may affect resistors
reliability.
• Surface temperature including self-heating must be kept below the maximum operating temperature.
• Avoid any water or heavy dust on resistors surface, which may cause electrical leakage, damage, overheating or corrosion.
Operating load conditions:
• Do not use the resistor with any higher than specified rated dissipation, rated current or rated voltage.
• Violation of the technical product specifications such as exceeding the specified dissipation will void the warranty.
• When the resistors are operated in ambient temperature above the rated temperature, the power rating must be derated according to
the derating curve.
• Verification and confirmation of performance characteristics of product, after on-board mounting, is advised.
Design of the PCB:
• The chip resistor shall be located to minimize any possible mechanical stress from deflection or board wrap.
• It is recommended to position the chip resistor in parallel to slits and perforations and as far away from slits, perforations, separation
points, screw holes, frames and edges of the PCB to avoid mechanical stress.
• Determine the shape and size of the solder pads to have proper amount of solder on the terminations as the amount of solder at the
terminations has a direct effect on resistance value and reliability of the resistor. The resistance value after soldering may change
depending on the size of land pattern, the wiring pattern or solder amount, make sure the effect of the change of the resistance value
before you use it.
• WE provide individual land patterns for each termination in the datasheet.
• Cracking of the solder fillet may occur with thermal cycling, because of mismatch of coefficients of thermal expansion between the
board and the component. Pad size, amount of solder, and amount of heatradiating from the PCB must be designed carefully.
• The parasitic inductance of the chip resistor and the wiring pattern may influence current detection under high frequency usage, make
sure the effect before you use it.
• The PCB design (e.g. land pattern design and grounding planes) must be evaluated for each individual circuit to achieve the optimal
soldering results.
Mounting:
• Adjust the bottom dead center of the mounting head not to press on the PCB surface to avoid any punctual pressure on component at
pick & place.
• When a highly active halogenous (chlorine,bromine, etc.) flux is used, the residues of flux may negatively affect resistor performance
and reliability.
Würth Elektronik eiSos GmbH & Co. KG
EMC & Inductive Solutions
Max-Eyth-Str. 1
74638 Waldenburg
Germany
Tel. +49 (0) 79 42 945 - 0
www.we-online.com
eiSos@we-online.com
CREATED CHECKED GENERAL TOLERANCE PROJECTION
METHOD
KaS PSL DIN ISO 2768-1m
DESCRIPTION TECHNICAL REFERENCE
WRIS-KWKB Thick Film Resistors KB06124700J304DAATP0000
ORDER CODE
561020132023
SIZE REVISION STATUS DATE (YYYY-MM-DD) BUSINESS UNIT PAGE
0612 001.001 Valid 2018-11-14 eiSos 4/6
This electronic component has been designed and developed for usage in general electronic equipment only. This product is not authorized for use in equipment where a higher safety standard and reliability standard is especially required or where a failure of the product is reasonably expected to cause severe personal injury or death, unless the parties have executed an agreement specifically governing such use. Moreover Würth Elektronik eiSos GmbH
& Co KG products are neither designed nor intended for use in areas such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control, ship control), transportation signal, disaster prevention, medical, public information network etc.. Würth Elektronik eiSos GmbH & Co KG must be informed about the intent of such usage before the design-in stage. In addition, sufficient reliability evaluation checks for safety
must be performed on every electronic component which is used in electrical circuits that require high safety and reliability functions or performance.