QUICK START GUIDE FOR DEMONSTRATION CIRCUIT 7888
SINGLE CELL LIEION BATTERY CHARGER WITH NTC
LTLJCUHIR
QUICK START GUIDE FOR DEMONSTRATION CIRCUIT 788B
SINGLE CELL LI-ION BATTERY CHARGER WITH NTC
3
QUICK START PROCEDURE
The charger can be evaluated using an actual Lith-
ium Ion battery or a battery simulator. The battery
simulator is faster because all battery state-of-
charge conditions can be quickly simulated.
A battery simulator consists of an adjustable power
supply with a load resistor across the power supply
output. The resistor value is selected that will pro-
vide approximately 1A when the power supply is set
for 2.5V and the power supply must provide at least
1.7A when adjusted for 4.4V. For this battery simu-
lator, a 2.5 Ohm, 10 Watt power resistor connected
to the output of a 5V, 2A bench supply will work
fine. The power supply can now sink and source
current, similar to a battery, and by changing the
power supply voltage, any battery state-of-charge
condition can be quickly simulated.
Begin circuit evaluation by moving the jumpers to
the appropriate positions. Move the Termination
Method jumper (JP1) to the ITERM (upper) position
to select minimum charge current termination.
Move the IDET jumper (JP4) to the 100mA (lower)
position, the ICHG-2 jumper (JP2) to the “C” (up-
per) position and the ICHG-1 jumper (JP3) to the
HIGH (upper) position. For this evaluation, disable
the NTC feature by placing the NTC jumper (JP5) in
the lower position. The charger is now set to charge
at 1A and use minimum charge current (IDET =
100mA) for charge termination.
With the input power supply and battery simulator
power supply adjusted to 0V, connect the input
power supply output to the VIN and GND, and the
battery simulator power supply output to the BAT
and GND terminals as shown in Figure 1. An amme-
ter or 100m current sense resistor can be placed
between the BAT terminal and the positive terminal
of the battery simulator to measure charge current.
Connect a 4½ digit DVM to the BAT and GND termi-
nals to measure battery voltage. Begin increasing
the input supply voltage, up to 5V. At approximately
3.8V (the undervoltage lockout threshold), the
CHRG LED will turn on and the preconditioning
trickle charge of 100mA will begin flowing. Adjust
the battery simulator power supply to 3V. At ap-
proximately 2.9V, the charge current will abruptly
increase to the programmed constant current of 1A.
Continue slowly increasing the battery simulator
power supply, thus simulating the Li-Ion battery ac-
cepting charge. As the battery simulator approaches
the float voltage of 4.375V, the charge current will
begin to drop as the charger begins the constant
voltage portion of the charge cycle. It is important to
keep the DC resistance between the charger output
and the battery to a minimum, otherwise the charge
current will begin dropping much sooner. When the
charger is in the constant voltage portion of the
charge cycle, small changes in the simulator power
supply voltage will result in relatively large changes
in charge current. When the charge current drops
below the IDET threshold of 100mA, the charge cur-
rent will drop to 0, the CHRG LED will go OFF and
the charge cycle will end. When timer termination is
selected (using JP1), the CHRG LED will go off
when the charge current drops below 100mA, but
the charge cycle will continue until the 3 hour timer
ends.
After the charge cycle has ended, if the battery volt-
age drops approximately 100mV, a recharge cycle
will begin. A recharge cycle is 50% (1.5 hours) of
the programmed time (provided timer termination is
selected).