ATA5575M2 Datasheet by Microchip Technology

.1 IIIEI.®
9217C–RFID–12/11
Features
Contactless power supply
Contactless read/write data transmission
Radio frequency fRF from 100kHz to 150kHz
128-bit EEPROM user memory: 16 Bytes (8 Bits each)
8-bit configuration memory
High Q-antenna tolerance due to built-in options
Applications
Animal ID, waste management, industrial identification
ISO/IEC 11784/785 compatibility
FDX-A
FDX-B
On-chip trimmed antenna capacitor
330pF ±3%
250pF ±3%
Mega pads 200µm x 400µm
Mega pads 200µm x 400µm with 25µm gold bumps for direct coil bonding
Other options:
Direct access mode
OTP functionality
Atmel ATA5575M2
Read/Write LF RFID IDIC 100kHz to 150kHz
DATASHEET
Q? Q? HHH HHH w Hfi A IIIEI.
2Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
1. Description
The Atmel® ATA5575M2 is a contactless read/write identification IC (IDIC®) for applications in the 100-kHz to 150-kHz
frequency band. A single coil connected to the chip serves as the IC's power supply and bi-directional communication interface.
This antenna coil together with the chip form a transponder or tag.
The on-chip 128-bit User EEPROM (16 bytes with 8 bits each) can be read and written byte-wise from a base station (reader).
Data is transmitted from the IDIC (uplink) using load modulation. This is achieved by damping the RF field with a resistive load
between the two terminals Coil 1 and Coil 2. The IC receives and decodes serial base station commands (downlink), which are
encoded as 100% amplitude-modulated (OOK) pulse-interval-encoded bit streams.
The Atmel ATA5575M2 is an EEPROM-based circuit. It is optimized for maximum read range. Programming is also possible but
the write range is limited.
The typical animal ID application conforming to ISO11784/85 is read-only and operates at 134.2kHz. The Atmel ATA5575M2
thus has to be locked after programming the animal-specific code.
2. System Block Diagram
Figure 2-1. RFID System Using Atmel ATA5575M2 Tag
3. Atmel ATA5575M2 - Functional Blocks
Figure 3-1. Block Diagram
Data
Reader
or
Base station
Atmel ATA5575
Power
Transponder
Coil interface
Controller
Memory
Memory
(136-bit EEPROM)
Modulator
Analog front end
Data-rate
generator
Write
decoder
POR
Coil 2
Coil 1
Controller
Test logic HV generator
Input register
Mode register
41m
3Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
4. Analog Front End (AFE)
The AFE includes all circuits which are connected directly to the coil terminals. The AFE generates the IC power supply and
handles bi-directional data communication with the reader. The AFE consists of the following blocks:
Rectifier to generate a DC supply voltage from the AC coil voltage
Clock extractor
Switchable load between Coil 1 and Coil 2 for data transmission from tag to the reader
Field-gap detector for data transmission from the base station to the tag
ESD protection circuitry
4.1 Data Rate Generator
The data rate of the Atmel ATA5575M2 is programmable to operate at RF/50 (FDX-A mode) and RF/32 (FDX-B mode).
4.2 Write Decoder
The write decoder detects the write gaps and verifies the validity of the data stream according to the Atmel® downlink protocol
(pulse-interval encoding).
4.3 HV Generator
This on-chip charge pump circuit generates the high voltage required for programming the EEPROM.
4.4 DC Supply
Power is supplied externally to the IDIC via the two coil connections. The IC rectifies and regulates this RF source and uses it to
generate its supply voltage.
4.5 Power-On Reset (POR)
The power-on reset circuit blocks the voltage supply to the IDIC until an acceptable voltage threshold has been reached. This,
in turn, triggers the default initialization delay sequence. During this configuration period of 98 field clocks, the ATA5575M2 is
initialized with the configuration data stored in EEPROM byte 16.
4.6 Clock Extraction
The clock extraction circuit uses the external RF signal as its internal clock source.
4.7 Controller
The control logic module executes the following functions:
Load mode register with configuration data from EEPROM byte 16 after power-on and during reading
Controls each EEPROM memory read/write access and handles data protection
Handle downlink command decoding, detecting protocol violations and error conditions
41m
4Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
4.8 Mode Register
The mode register maintains a readable shadow copy of the configuration data held in byte 16 of the EEPROM. It is continually
refreshed during read mode and (re-)loaded after every POR event or reset command. Depending on the version, upon leaving
the Atmel® factory site, the configuration data is pre-programmed according to Table 10-1 on page 18 and Table 10-4 on page
20.
4.9 Modulator
The modulator encodes the serialized EEPROM data for transmission to a tag reader or base station. Two types of encoding
are implemented: Differential Biphase and FSK.
4.10 Memory
The memory is a 136-bit EEPROM arranged in 17 bytes of 8 bits each. Programming takes place on a byte basis meaning a
complete byte is programmed with a single command.
Byte 16 contains the mode/configuration data which is otherwise not transmitted during regular-read operations.
A special combination of bits in byte 16 (see Table 5-1 on page 5) locks the whole memory. Once locked, the memory (including
byte 16 itself) is not reprogrammable through the RF field again.
Figure 4-1. Memory Map
1………………....…………….8
Configuration dataByte 16
User data Byte 15
User data Byte 14
User data Byte 13
User data Byte 12
User data Byte 11
User data Byte 10
User data Byte 9
User data Byte 8
User data Byte 7
User data Byte 6
User data Byte 5
User data Byte 4
User data Byte 3
User data Byte 2
User data Byte 1
User data Byte 0
8 bits
Not transmitted
41m
5Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
5. Operating the Atmel ATA5575M2
5.1 Configuration
The Atmel® ATA5575M2 is mainly designed for ISO11784/11785 applications. It supports FDX-A and FDX-B mode (see also
Figure 7-1 on page 14 for the structure of a FDX-B telegram typically used for animal ID applications). The configuration
register, byte 16, enables the customer to configure the chip according to the individual application.
In delivery state the default configuration is memory reprogrammable, read user data in diff. biphase RF/32 and ID length 128
bit which leads to the byte value '00001001b'.
5.1.1 Lock-bits
The lock bits of the Configuration register are the bits 1 to 5 of the configuration byte and are able to prevent the whole memory
of the Atmel ATA5575M2 from reprogramming.
As long as the lock bits are set to '00000b' the memory is alterable and the device can be programmed by the customer. In this
case the Atmel ATA5575M2 sends out dummy data (all digits set to '0' in the programmed modulation scheme; see Section
5.3.3 “Dummy Data” on page 7) after Reset.
If the lock bits are set to '00001b' the memory is still alterable but in difference to the first option the Atmel ATA5575M2 sends
out the programmed user data in the modulation scheme defined with bit 7.
By setting the lock bits to '01101b' the whole memory is locked and cannot be altered. After Reset the Atmel ATA5575M2 enters
regular-read mode and sends out the programmed user data in the configured way.
All other combinations of bit 1 - bit 5 are not defined and may lead to malfunction of the IC.
Table 5-1. Atmel ATA5575M2: Byte 16 Configuration Register Mapping
12345678
0
ID Length
0 64 bits (96 bits for FSK2 RF/50 coding (2))
1128 bits 1)
Modulation
0 Differential bi-phase RF/32 (1)
1 FSK2 RF/50 (2)
Fixed ‘0’
Lock-bits
0 0 0 0 1 Memory reprogrammable
0 1 1 0 1 Memory locked
- otherwise - unassigned
Bit 6 must always be at '0', otherwise a malfunction will appear
Notes: 1. Setting for ISO 11785 FDX-B
2. Setting for ISO 11785 FDX-A
41m
6Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
5.1.2 Modulation
The modulator consists of data encoders for the following types of modulation.
5.1.3 ID Length
The Atmel® ATA5575M2 offers settings for different ID lengths. If bit 8 of byte 16 is set to '1', the ID length is 128 bits.
Depending on the modulation scheme, resetting bit 8 of byte 16 to '0' leads either to the ID length of 64 bit with differential bi-
phase coding or to the ID length of 96 bit with FSK2 coding respectively.
5.2 Animal ID and Traceability
During Atmel’s production process the Atmel ATA5575M2 will be pre-configuered in the ISO11784/11785 FDX-B mode and a
unique ID (UID) will be stored in the user memory. The unique ID consists of Atmel’s production information like lot number,
wafer number, and die-on-wafer number. With these data each chip can be traced and concurrently each chip has its own
unique ID for identification purposes(1).
For ISO11784/11785 FDX-B telegrams please refer to Section 7. “Examples for Programming the ATA5575M2” on page 14.
Section 10.2 “ATA5575M2 Configuration on Delivery” on page 18 describes how the unique ID is formed based on Atmel
production information.
Note: 1. Please note that this traceability data is only for production control and does not conform with any ISO, national or
other regulations.
5.3 Tag-to-reader Communication (Uplink)
Immediately after entering the reader field, generating the internal supply voltage and the analog POR, in the deliv-
ery state the tag cycles its data stored in EEPROM by load modulation according to the configuration setting. This
resistive load modulation can be detected at the reader device.
5.3.1 Regular-read Mode
In regular-read mode data from the memory is transmitted in series, starting with byte 0, bit 1, up to the last byte, bit 8. Last byte
is defined in bit 8 of byte 16, ID Length. When the last bit of the last byte (defined by ID length) has been read, data transmission
restarts with byte 0, bit 1.
The device enters regular-read mode in delivery state (lock bits set to '00001b' or set to '01101b'; please refer to Section 5.1.1
“Lock-bits” on page 5).
Last byte is 15, when ID Length = 1 (128 bit).
For differential bi-phase modulation, the last byte is 7 when ID Length = 0 (64 bits) is chosen.
For FSK2 RF/50 modulation, the last byte is 11 when ID length = 0 (96 bits) is chosen.
Every time the Atmel ATA5575M2 enters regular or byte read mode, the first bit transmitted is a logical '0'. The data stream
starts with bit 1 of byte 0 or bit 1 of the addressed byte.
Table 5-2. Atmel ATA5575M2: Types of Modulation
Symbol Direct Data Output Encoding
FSK2 RF/50 FSK/10 – FSK/8 0 = RF/10 1 = RF/8
Differential bi-phase Transition at each bit start
0 creates an additional mid-bit change
H n h u aiiL 41m
7Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
Figure 5-1. Examples of Different ID Length Settings
5.3.2 Byte-read Mode
With the direct access command, only the addressed byte is read repetitively. This mode is called byte-read mode. Direct
access is entered by transmitting the opcode ('10'), a single 0 bit, and the requested 5-bit byte address.
5.3.3 Dummy Data
The dummy data are a predefined bit sequence of all bits set to value '0'. This sequence is read out instead of the data stored in
the user memory if the lock bits are set to '00000b'.
5.4 Reader-to-tag Communication (Downlink)
Data is transmitted to the tag by interrupting the RF field with short field gaps (on-off keying) according to the Atmel® ATA5577
fixed-bit-length protocol (downlink mode). The duration of these field gaps is, for example, 100µs. The time between two gaps
encodes the 0/1 information to be transmitted (pulse interval encoding). The time between two gaps is nominally 25 field clocks
for a 0 and 58 field clocks for a 1. When there is no gap for more than 64 field clocks after a previous gap, the Atmel
ATA5575M2 exits the downlink mode. The tag starts with the command execution if the correct number of bits were received. If
an error condition occurs, the Atmel ATA5575M2 does not continue command execution and enters read mode depending on
the setting of the lock bits.
The initial gap is referred to as the start gap. This triggers reader-to-tag communication. The start gap may need to be longer
than subsequent gaps - so-called write gaps - in order to be detected reliably.
A start gap is accepted at any time after the mode register has been loaded (1ms).
Figure 5-2. Start of Reader-to-tag Communication (Downlink)
0
Loading byte 16
Byte 6 Byte 7 Byte 1Byte 0Byte 0
0
ID Length = ‘0’
with diff. Bi-phase
coding
ID Length = ‘0’
with FSK2 coding Loading byte 16
Byte 10 Byte 11 Byte 1Byte 0Byte 0
0
Loading byte 16
Byte 14 Byte 15 Byte 1Byte 0Byte 0
ID Length = ‘1’
Write modeRead mode
S
gap
W
gap
Note: All absolute times are given under the assumption TC = 1/1C = aps (IC = 125kHz) \HIF T WV M AA A IIIEI.
8Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
All absolute times assume TC = 1/fC = 8µs (fC = 125kHz)
5.4.1 Downlink Data Protocol
The Atmel® ATA5575M2 expects to receive a dual bit opcode as a part of a reader command sequence. There are three valid
opcodes and overall five different commands (please refer to Figure 5-4 on page 9):
The RESET opcode '00' starts an initialization cycle
A single '10' opcode (Read ID) leads to reading the ID out of the EEPROM memory. This is suitable to check the
programmed user data if the memory is not locked already. The opcode '10' precedes all downlink operations for writing
data into the EEPROM
The opcode '11' reads the upper bytes when ID length (bit 8 of byte 16) is set to '0'
If ID length is set to '1' opcode '11' is the same than opcode '10'
The Write Byte requires the opcode '10', a '0' bit, 8 data bits and the 5-bit address (16 bits total)
For Direct access, the opcode '10', a '0' bit and a 5-bit address (8 bits total), is required
Note: The data bits are read in the same order as written.
Figure 5-3. Complete Write Sequence
Table 5-3. Downlink Data Decoding Scheme
Parameter Remark Symbol Min. Typ. Max. Unit
Start gap Sgap 815 50 TC
Write gap Wgap 810 20 TC
Write data coding
(gap separation)
0 data d018 25 33 TC
1 data d150 58 65 TC
Note: All absolute times are given under the assumption TC = 1/fC = 8µs (fC = 125kHz)
Write mode Read modeRead mode
ProgrammingByte addressByte data
Start gap
Configuration
loading
POR
Opcode
‘0’
as: 41m
9Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
5.5 Programming
When all necessary information has been received by the ATA5575M2, programming may proceed. There is a clock delay
between the end of the writing sequence and the start of programming.
Typical programming time is 5.6ms. This cycle includes a data verification read to grant secure and correct programming. After
programming is successfully executed, the ATA5575M2 enters byte-read mode, transmitting the byte just programmed.
If the command sequence is validated, the new data is programmed into the EEPROM memory.
Each programming cycle consists of four consecutive steps: erase byte, erase verification (data = 0), programming,
programming verification (corresponding data bits = 1).
Figure 5-5. Coil Voltage after Programming a Byte
Figure 5-4. ATA5575M2 Command Formats
OP
Write byte 1001 Data 8 4 Addr 0
Direct access 1004 Addr 0
Read ID 1 0
Read upper bytes 1 1
Reset command 0 0
Read programmed
memory byte Read ID Read ID5.6 ms
(Regular read mode)(Byte read mode)Programming and
data verification
Write data to tag
V
Coil 1 - Coil 2
41m
10Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
6. Error Handling
Several error conditions can be detected to ensure that only valid bits are programmed into the EEPROM. There are two error
types which result into two different actions.
6.1 Errors During Command Sequence
The following detectable errors could occur when sending a command sequence to the Atmel® ATA5575M2:
The wrong number of field clocks between two gaps (i.e., not a valid 1 or 0 pulse stream)
The number of bits received in the command sequence is incorrect
6.2 Errors Before/During Programming of EEPROM
If the command sequence was received successfully, the following errors may still prevent programming:
The lock bits of the memory are already set
If the memory is locked, programming is not possible. The Atmel® ATA5575M2 enters byte-read mode, continuously
transmitting the currently addressed byte.
If a data verification error is detected after programming of an executed data byte, the tag will stop modulation
(modulation defeat) until a new command is transmitted.
Table 6-1. Bit Counts of Command Sequences
Command Number of Bits
Write byte 16
Direct access 8
Read ID 2
Read upper bytes 2
Reset command 2
A IIIEl
11Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
Figure 6-1. Atmel® ATA5575M2 Functional Diagram
Byte-read mode
Program and verify
Write
Check Write protection
Check Number of bits
Command decode
Start
gap
Write
OP(1p)
Reset
Modulation
defeat
fail data = unchanged
fail data = unchanged
Gap
Command mode
Read ID
Set-up modes
Power-on reset
Regular-read mode /
Read dummy data
okData verification failed data = new
Read ID
Read upper bytes
OP (00)
Gap
OP(10) Read ID
OP(11) Read upper bytes
OP(10) Direct access
12Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
Figure 6-2. Example of Differential Bi-phase Coding with Data Rate RF/32
RF-field
Modulator signal
Data stream
1
16 FC
16 FC
Data rate =
Bi-phase coded
64 Field Clocks (FC)
00110
1
111
116 17
1
32
17
16
32
32
16
32
17
16
32
17
16
32
17
16
13Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
Figure 6-3. Example of FSK2 Coding with Data Rate RF/50, Subcarrier f0= RF/10, f1=RF/8
RF-field
Modulator signal
Data stream
100110
10 18
Data rate =
50 Field Clocks (FC)
1
f
0
= RF/10,
f
1
= RF/8
lllll\llllllll EI[|,|||| 41m
14Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
7. Examples for Programming the ATA5575M2
Animal ID is a typical application with ISO11784/11785. The following describes the data structure of an FDX-B telegram and a
flow for programming ATA5575M2 using sample data.
Figure 7-1. ATA5575M2: Structure of the ISO 11785 FDX-B Telegram
Notes:
Except for the header, every 8 bits are followed by one control bit (1), to prevent the header from recurring.
All data is transmitted LSB first.
Country codes are defined in ISO 3166
The bits reserved for future use (RFU) are all set to 0.
If the data block flag is not set, the trailer bits are all set to 0.
CRC is performed on the 64-bit identification code without the control bits. The generator polynomial is
P(x) = x16 +x
12 +x
5+ 1. Reverse CRC-CCITT (0x 8 408) is used. The data stream is LSB first.
Example data for programming Atmel ATA5575M2 in FDX-B mode:
Animal flag: 1
RFU: 0
Data block flag: 0
Country code: 999
Unique number: 123456789
Trailer: 0
41m
15Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
Table 7-1. Atmel® ATA5575M2: Programming with FDX-B Example Data
Base Station Atmel ATA5575M2
Field on for t = 5ms POR and regular-read mode
Command 00 Reset
Command 10 0 0000 1001 10000 Programming byte 16 with ‘09h’ (FDX-B mode, memory
reprogrammable)
Command 10 0 0000 0000 00000 Programming byte 0 with ‘00h’
Command 10 0 0011 0101 00001 Programming byte 1 with ‘35h’
Command 10 0 0001 1011 00010 Programming byte 2 with ‘1Bh’
Command 10 0 0011 1110 00011 Programming byte 3 with ‘3Eh’
Command 10 0 1101 0111 00100 Programming byte 4 with ‘D7h’
Command 10 0 1000 0010 00101 Programming byte 5 with ‘82h’
Command 10 0 0000 0111 00110 Programming byte 6 with ‘07h’
Command 10 0 1001 1111 00111 Programming byte 7 with ‘9Fh’
Command 10 0 1000 0000 01000 Programming byte 8 with ‘80h’
Command 10 0 0100 0000 01001 Programming byte 9 with ‘40h’
Command 10 0 0110 1110 01010 Programming byte 10 with ‘6Eh’
Command 10 0 1001 1000 01011 Programming byte 11 with ‘98h’
Command 10 0 1010 1000 01100 Programming byte 12 with ‘A8h’
Command 10 0 0000 0100 01101 Programming byte 13 with ‘04h’
Command 10 0 0000 0010 01110 Programming byte 14 with ‘02h’
Command 10 0 0000 0001 01111 Programming byte 15 with ‘01h’
Command 10 Read ID
Field on for t = 50ms
Read and verify FDX-B data Send FDX-B data
Command 10 0 0110 1001 10000 Programming byte 16 with ‘69h’
(FDX-B mode, memory locked)
Command 00 Reset
Field on for t = 50ms
Read and verify FDX-B data Send FDX-B data
Note: For data retention please refer to Sechon 9. “E‘eclncal Charaderisfics” on page 16. A IIIEI.
16Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
8. Absolute Maximum Ratings
Stresses beyond those listed under “Absolute Maximum Ratings” may cause permanent damage to the device. This is a stress rating
only and functional operation of the device at these or any other conditions beyond those indicated in the operational sections of this
specification is not implied. Exposure to absolute maximum rating conditions for extended periods may affect device reliability.
Parameters Symbol Value Unit
Maximum DC current into Coil1/Coil2 Icoil 20 mA
Maximum AC current into Coil1/Coil2
f = 125kHz Icoil p 20 mA
Power dissipation (dice) (free-air condition, time of
application: 1s) Ptot 100 mW
Electrostatic discharge maximum to ANSI/ESD-STM5.1-2001
standard (HBM) Vmax 2000 V
Operating ambient temperature range Tamb –40 to +85 °C
Storage temperature range Tstg –40 to +150 °C
Note: For data retention please refer to Section 9. “Electrical Characteristics” on page 16.
9. Electrical Characteristics
Tamb = +25°C; fcoil = 125kHz; unless otherwise specified
No. Parameters Test Conditions Symbol Min. Typ. Max. Unit Type*
1RF frequency range fRF 100 125 150 kHz
2.1
Supply current (without
current consumed by the
external LC tank circuit)
Tamb = 25°C (1) IDD 1.5 3µA T
2.2 Read – full temperature
range 2 5 µA Q
2.3 Programming – full
temperature range 25 µA Q
3.1 Coil voltage (AC supply)
Read mode and write
command 2) Vcoil pp 6 Vclamp V Q
3.2 Program EEPROM(2) 16 Vclamp V Q
4Start-up time Vcoil pp = 6V tstartup 1.1 ms Q
5.1 Clamp 3mA current into Coil1/2 Vpp 15 18 21 V T
5.2 20mA current into Coil1/2 Vpp 17 20 24 V T
6.1
Modulation parameters
3mA current into Coil1/2
and modulation ON Vpp 2 3 4 V T
6.2 20mA current into Coil1/2
and modulation ON Vpp 4.5 58.5 V T
6.3 Thermal stability of
modulation parameter Vp/Tamb –1 mV/°C Q
*) Type means: T: directly or indirectly tested during production; Q: guaranteed based on initial product qualification data
Notes: 1. IDD measurement setup: EEPROM programmed to 00 ... 000 (erase all); chip in modulation defeat.
2. Current into Coil1/Coil2 is limited to 10mA.
3. Since the EEPROM performance is influenced by assembly processes, Atmel cannot confirm the parameters for -DDW
(tested die on unsawn wafer) delivery.
4. See Section 10. “Ordering Information” on page 18.
A IIIEI.
17Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
7.1 Clock detection level Vcoil pp = 8V Vclkdet 400 550 750 mV T
7.2 Gap detection level Vcoil pp = 8V Vgapdet med 400 550 750 mV T
8Programming time
From last command gap
to re-enter read mode
(64 + 648 internal clocks)
Tprog 55.7 6ms T
9Endurance Erase all/Write all(3) ncycle 100000 Cycles Q
10.1
Data retention
Top = 55°C(3) tretention 10 20 50 Years Q
10.2 Top = 150°C(3) tretention 96 hrs T
10.3 Top = 250°C(3) tretention 24 hrs Q
11.1 Resonance capacitor Mask option(4)
Vcoil pp = 1V Cr
320 330 340 pF T
11.2 242 250 258
9. Electrical Characteristics (Continued)
Tamb = +25°C; fcoil = 125kHz; unless otherwise specified
No. Parameters Test Conditions Symbol Min. Typ. Max. Unit Type*
*) Type means: T: directly or indirectly tested during production; Q: guaranteed based on initial product qualification data
Notes: 1. IDD measurement setup: EEPROM programmed to 00 ... 000 (erase all); chip in modulation defeat.
2. Current into Coil1/Coil2 is limited to 10mA.
3. Since the EEPROM performance is influenced by assembly processes, Atmel cannot confirm the parameters for -DDW
(tested die on unsawn wafer) delivery.
4. See Section 10. “Ordering Information” on page 18.
41m
18Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
10. Ordering Information
10.1 Available Order Codes
Atmel ATA5575M2330-DDB
Atmel ATA5575M2330-DBB
New order codes will be created by customer request if order quantities exceed 250k pieces.
10.2 ATA5575M2 Configuration on Delivery
On delivery Atmel’s production information is stored in EEPROM with the FDX-B data structure as described in Figure 7-1 on
page 14.
The user data contains Atmel’s lot and production information as described in Table 10-2. With 38 bits, 12 decimals in the range
from 0 to 274 877 906 943 can be formed. The following Atmel production information is stored within these 12 decimal places.
ATA5575M2 ccc -xxx PackageDrawing
DDB 6” sawn wafer on foil with ring, thickness 150µm
(approx. 6mil) Figure 11-1 on page 21
DBB 6” sawn wafer on foil with ring and gold bumps 25µm,
thickness 150µm (approx. 6mil) Figure 11-2 on page 22
DBN Die on sticky tape with gold bumps 25µm,
thickness 280µm
Sticky Tape: 3M 7419
Figure 11-3 on page 23
On-chip capacity value in pF
250 (planned)
330
Table 10-1. ATA5575M2: Configuration on Delivery
Byte Address Value Comment
User data byte 0 to byte 15 0b 0 0000 to 0b 0 1111 Variable data Unique ID within a FDX-B telegram
Configuration (byte 16) 0b 1 0000 0x 09 Send FDX-B telegram with user data
byte 0 to byte 15
Table 10-2. Atmel ATA5575M2: Meaning of the Digits of Unique Number in Delivery State
Decimal 11 10, 9 8765, 4, 3, 2 1, 0
Denotation Header CID ICR Y Q NNNN Wafer#
Range [dec] 1 (fixed) 1-99 0-9 0-9 1-4 0-9999 1-25
For example 104 0910164 12
41m
19Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
Notes:
First decimal Header is always fixed at ‘1’
CID denotes the chip ID and is set to ‘4’ for Atmel® ATA5575M2
ICR stands for the revision and/or foundry version of the IC
YQNNNN gives the Atmel lot information
Y: alphanumeric 0, …, 9
Q: Characters F, G, H and J - are transformed to 1, …, 4
NNNN: Alphanumeric consecutive number 0, …, 9999
Wafer# describes a lot's wafer numbers; alphanumeric 1, …, 25
The Unique Number will then calculated to:
Unique Number = Header*1011 + CID*109 + ICR*108 + Y*107 + Q*106 + NNNN*102 + Wafer#
For the example given in Table 10-2 on page 18 the Unique Number is 104 091 016 412
With the 24 trailer bits 8 decimals in the range 0 to 16 777 216 can be established. The following Atmel® production information
is stored within these 8 decimal places.
Notes:
The first 3 decimals of the Header are always fixed: '111'
Die on wafer (DW): Consecutive number of die on wafer: 1 to 99 999
The Trailer is then calculated to:
Trailer = Header*105 + DW
With the example given in Table 10-3 the Trailer is 11 109 127
Table 10-3. Atmel ATA5575M2: Meaning of the Digits of Trailer Bits in Delivery State
Decimal 7, 6, 5 4, 3, 2, 1, 0
Denotation Header Die-on-wafer no. (DW)
Range [dec] 111 (fixed) 0 to 99 999
For example 111 09 127
41m
20Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
10.2.1 ATA5575M2 Example for Memory Content on Delivery
The following describes an example of the memory content after Atmel’®s production.
CID: 4
ICR: '00b'
Lot number: 9F0164
Wafer number: 12
Die on wafer: 9.127
Unique Number = 1 × 1011 + 4 × 109 + 0 × 108 + 9 × 107 + 1 × 106 + 0164 × 102 +
12 = 104 091 016 412
Trailer = 111 × 105 + 9,127 = 11 109 127
With the sample data above the FDX-B telegram fields are:
Animal flag ( 1 bit) = ‘1b’ fixed
RFU (14 bit) = ’00 0000 0000 0000b’ fixed
Data block flag (1 bit) = ‘0b’ fixed
Country code (10 bit) = 999 (= '11 1110 0111b') fixed
Unique number (38 bit) = 104 091 016 412
CRC (16 bit) = 39 505
Trailer (24 bit) = 11 109 127
Table 10-4. ATA5575M2: Example of Memory Content on Delivery
Byte# 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16
Meaning Header
Header
/
Unique
Number
Unique
number
Unique
number
Unique
number
Unique
number
Unique
number
/
Country
Code
Country
code
Data
Block
Flag /
RFU
RFU
RFU /
Animal
Flag /
CRC
CRC CRC /
Trailer Trailer Trailer Trailer Confi-
guration
Value
[hex] 00 27 73 BB 94 F2 37 9F 80 40 71 55 9F 07 07 2B 09
41m
21Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
11. Package Information
Figure 11-1. 6” Wafer on Foil with Ring
TITLE DRAWING NO. REV.
Package Drawing Contact:
packagedrawings@atmel.com 9.920-6716.01-4 3
ATA5575MYxxx-DDB
Dimensions
1 330
1
2
250
330
2 250
Option
Y
Option
xxx
01/18/11
20:1
Die Dimensions
Dimensions in mm
specifications
according to DIN
technical drawings
Orientation on frame
Ø 227.7
212
Ø194.5
Ø150
212
87.5
86.5
Wafer ATA5575MYxxx-DDB
6" Wafer frame, plastic
thickness 2.5mm
UV Tape Adwill D176
Label:
Qty:
Wafer no:
Lot no:
Prod: ATA5575MYxxx-DDB
59.5 63.6
4B
B
AØ3
A
0.15±0.012
0.966
0.402
0.4
(0.08)
0.326
0.04 × 45°
(0.08) 0.21
0.2
0.946
C2 C1
41m
22Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
Figure 11-2. 6” Wafer on Foil with Ring and Gold Bumps 25µm
TITLE DRAWING NO. REV.
Package Drawing Contact:
packagedrawings@atmel.com 9.920-6716.02-4 3
ATA5575MYxxx-DBB
Dimensions
01/18/11
20:1
Die Dimensions
Dimensions in mm
specifications
according to DIN
technical drawings
Orientation on frame
Ø 227.7
212
Ø194.5
Ø150
212
87.5
86.5
Wafer ATA5575MYxxx-DDB
6" Wafer frame, plastic
thickness 2.5mm
UV Tape Adwill D176
Label:
Qty:
Wafer no:
Lot no:
Prod: ATA5575MYxxx-DDB
59.5 63.6
4B
B
AØ3
A
0.966
0.402
0.4
(0.08)
0.326
0.04 × 45°
(0.08) 0.21
0.2
0.946
C2 C1
0.155±0.014
0.025±0.005
0.15±0.012
0.175±0.017
(Au bump)
0.005±0.002
(BCB coating)
1 330
1
2
250
330
2 250
Option
Y
Option
xxx
A IIIEI.
23Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
Figure 11-3. Die on Sticky Tape with Gold Bumps 25µm
TITLE DRAWING NO. REV.
Package Drawing Contact:
packagedrawings@atmel.com 9.800-5109.01-4 2
ATA5575MYxxx-DBN
Dimensions
01/18/11
specifications
according to DIN
technical drawings
20:1
Die Dimensions
(0.08)
C2 C1
0.946
0.21
0.2
(0.08)
0.4
0.402
0.966
(BCB coating)
0.285±0.0135
0.005±0.0015
(Au bump)
0.025±0.005
0.305±0.017
0.28±0.012
8±0.1
8.4
reel Ø180
0.326
0.04 × 45°
Glue
2mm min.
0.15 A
A
Direction of unwinded tape Yellow translucent tape
’’X’’
’’X’’
Specification Sticky tape
Dimensions in mm
Label acc. ’’Packaging and Packing Spec.’’
1 330
1
2
250
330
2 250
Option
Y
Option
xxx
41m
24Atmel ATA5575M2 [DATASHEET]
9217C–RFID–12/11
12. Revision History
Please note that the following page numbers referred to in this section refer to the specific revision mentioned, not to this
document.
Revision No. History
9217C-RFID-12/11 Set datasheet from Preliminary to Standard
9217B-RFID-05/11
Section 1 “Description” on page 1 changed
Section 4 “Analog Front End (AFE) on pages 3 to 4 changed
Section 5 “Operating the Atmel ATA5575M2” on pages 5 to 9 changed
Section 6.2 Errors Before/During Programming of EEPROM” on page 11 changed
Section 8 “Absolute Maximum Ratings” on page 16 changed
Section 9 “Electrical Characteristics” on page 16 changed
Section 10.2 “Atmel ATA5575M2 Configuration on Delivery” on pages 18 to 19 changed
A [IIEL ‘ Enabling Unlimited Possibilities”
Atmel Corporation
2325 Orchard Parkway
San Jose, CA 95131
USA
Tel: (+1) (408) 441-0311
Fax: (+1) (408) 487-2600
www.atmel.com
Atmel Asia Limited
Unit 01-5 & 16, 19F
BEA Tower, Millennium City 5
418 Kwun Tong Roa
Kwun Tong, Kowloon
HONG KONG
Tel: (+852) 2245-6100
Fax: (+852) 2722-1369
Atmel Munich GmbH
Business Campus
Parkring 4
D-85748 Garching b. Munich
GERMANY
Tel: (+49) 89-31970-0
Fax: (+49) 89-3194621
Atmel Japan G.K.
16F Shin-Osaki Kangyo Building
1-6-4 Osaki
Shinagawa-ku, Tokyo 141-0032
JAPAN
Tel: (+81) (3) 6417-0300
Fax: (+81) (3) 6417-0370
© 2011 Atmel Corporation. All rights reserved. / Rev.: 9217C–RFID–12/11
Disclaimer: The information in this document is provided in connection with Atmel products. No license, express or implied, by estoppel or otherwise, to any intellectual property right is granted by this
document or in connection with the sale of Atmel products. EXCEPT AS SET FORTH IN THE ATMEL TERMS AND CONDITIONS OF SALES LOCATED ON THE ATMEL WEBSITE, ATMEL ASSUMES
NO LIABILITY WHATSOEVER AND DISCLAIMS ANY EXPRESS, IMPLIED OR STATUTORY WARRANTY RELATING TO ITS PRODUCTS INCLUDING, BUT NOT LIMITED TO, THE IMPLIED
WARRANTY OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, OR NON-INFRINGEMENT. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT,
CONSEQUENTIAL, PUNITIVE, SPECIAL OR INCIDENTAL DAMAGES (INCLUDING, WITHOUT LIMITATION, DAMAGES FOR LOSS AND PROFITS, BUSINESS INTERRUPTION, OR LOSS OF
INFORMATION) ARISING OUT OF THE USE OR INABILITY TO USE THIS DOCUMENT, EVEN IF ATMEL HAS BEEN ADVISED OF THE POSSIBILITY OF SUCH DAMAGES. Atmel makes no
representations or warranties with respect to the accuracy or completeness of the contents of this document and reserves the right to make changes to specifications and products descriptions at any time
without notice. Atmel does not make any commitment to update the information contained herein. Unless specifically provided otherwise, Atmel products are not suitable for, and shall not be used in,
automotive applications. Atmel products are not intended, authorized, or warranted for use as components in applications intended to support or sustain life.
Atmel®, logo and combinations thereof, and others are registered trademarks or trademarks of Atmel Corporation or its subsidiaries. Other terms and product
names may be trademarks of others.