ASTRON Electronic GmbH
About
ASTRON Electronic GmbH is an EMS service provider founded in 1997 by employees and partners in the south of Carinthia/Austria and privately owned until today. We are specialized in the assembly of prototypes, single pieces up to tiny series (max. 100 000 components per production order). Our customers love us for the high quality, perfect workmanship and short delivery times, which is why our assembly is realized with flexible automatic assembly machines with almost no restrictions on the size and technology of the PCB, as well as the size and shape of the components. Soldering is done with a vapor phase soldering machine with vacuum module to reduce voids.
Certification of employees:
As you can see on our homepage in the section OUR TEAM, we have set the goal to train all our employees to become certified IPC specialists of IPC-A-610 and IPC 7711B/7721B. In the meantime, we have also been able to add J-STD-001 Certified IPC Specialists to our team. The new or biennial recertification of all employees is carried out by in-house IPC trainers.
On our homepage you can see in the INQUIRY section which data we need to prepare an offer, in the SERVICE section you can find information about the areas in which we can support you and in the area CERTIFICATES, AWARDS you will find our ISO certifications for EN ISO 9001, EN ISO 14001 and EN ISO 45001 as well as information about our awards at Austria's Leading Companies.