Digi-Key Corporation Broadens Line Card with Lattice MachXO2 Programmable Logic Devices

THIEF RIVER FALLS, Minnesota, USA - September 29, 2011

Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced the addition of Lattice’s MachXO2 Programmable Logic Devices.

Lattice Semiconductor's MachXO2 family of infinitely reconfigurable Programmable Logic Devices (PLDs) offers designers of low density PLDs an unprecedented mix of low cost, low power and high system integration in a single device. Combining an optimized look-up table (LUT) architecture with 65 nm embedded Flash process technology, the MachXO2 family delivers an increase in logic density, an increase in embedded memory, and a reduction in static power compared to the prior generation, the MachXO PLD family.

The MachXO2 family offers system designers the benefits of increased system integration, improved system robustness and reduced static power consumption. In addition, the MachXO2 family includes hardened implementations of some of the most popular functions used in system applications (telecom infrastructure, computing, high end industrial, high end medical, etc.) and consumer applications (smart phones, GPS devices, mobile computing, digital cameras, etc.). Through the provision of these features, the MachXO2 family offers designers a "Do-it-All PLD" for system applications.

Lattice’s MachXO2 Programmable Logic Devices are available for purchase now on Digi-Key's global websites.

About Digi-Key Corporation

Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.