Digi-Key Corporation Announces the Expansion of Cornell Dubiliers Snap-In Product Line

THIEF RIVER FALLS, Minnesota, USA - April 13, 2011

Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced the addition of aluminum electrolytic snap-in capacitors from Cornell Dubilier.

The entire addition consists of over 650 part numbers from the 380LX, 381LX, 382LX, 383LX, 381LR, SLP and SLPX series. These seven series of General Purpose and Low ESR capacitors come in 2-, 4-, or 5-pin configurations and are targeted for next generation switching power supplies, DC filtering circuits in inverters, and motor drive applications. CDE snap-in aluminum electrolytic capacitors have a wide range of capacitance values and voltage ratings with exceptional ripple current specifications.

These new capacitors are available for purchase now on Digi-Key's global websites.

Digi-Key Corporation focuses on providing customers with superior service, which includes product selection and availability, on-time delivery, and responsiveness. Using leading-edge processes and state-of-the-art technologies, Digi-Key serves a global customer base from its 600,000 square foot facility in Thief River Falls, Minnesota, USA.

About Digi-Key Corporation

Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.

About Cornell Dubilier Electronics

Cornell Dubilier is the source for capacitors that transform your applications to success stories. It excels with aluminum electrolytic, mica, motor run and AC and DC plastic film capacitors. Cornell Dubilier only makes capacitors and has been doing it for almost 100 years. The world leaders in welders, UPS systems, motors, drives, avionics, power and military electronics and medical lasers are prominently among its more than 33,000 customers.